Part Number: MAX3221 Hi everyone
I tested according to the recommended circuit diagram in the specification, the chip 12 and 16 pins are connected to 3.3V, when the chip 8 and 13 pins are connected to the 232 serial port of the computer, the output voltage…
Part Number: MAX3221E Hi Team,
We would like to know the transmission distance at the following conditions.
Our expectation is 15m as specified in RS232C.
-VCC=3.3V
-Data rate=250kbps
And, could you please let us know “Transmission distance vs Data…
Part Number: MAX3221 When IC is interfaced with L&T Energy Meter, Meter_TX Signal is attaining 3.48V & -4.2V rather than reaching +5.5V & -5.5V levels. I'm attaching Scope Output for your reference as well as Energy Meter - MAX 3221 Schematic for your…
Part Number: MAX3221 Hi team.
My customer is designing the layout for MAX3221.
I guess they have to care about below:
Parallel and equal length wiring for the Dout Rin.
For DIN and Rout, creepage distance should be secured atleast twice the line width…
Part Number: MAX3221E Other Parts Discussed in Thread: TRSF3221E Hi Team,
I am using MAX3221EIPWR in my design for UART interface which is used for board console terminal. My baudrate requirement is 921600 and the IC doesn't support this baudrate. Can you…
Part Number: MAX3221 Guys, does TI have the min and max data of tPLH, tPHL base on 3.3V or 5V ? D atasheet just show the typ. data as below picture.
Thanks in advance!
Part Number: MAX3221 When I asked the below question to the expert
we tried to connect the VCM voltage to the ECGP/ECGN for the accurate ADC input.
1. is it ok for the system?
2. now we are facing lead-off function for this system when we use VCM
Please…
Part Number: MAX3221 Hi team, I'd like to know about the automatic power down. Could you tell me about the time to output when switching from Automatic power down to normal operation? I think the automatic power down is switched to normal mode by the…
Part Number: MAX3221
Hi team, When auto power-down, how much is the Icc when EN is High or Low? I'd like to know if the Icc changes when the receiver is Enable or disable. Sincerely. Kengo.