Part Number: MAX3221 Hi team, I'd like to know about the automatic power down. Could you tell me about the time to output when switching from Automatic power down to normal operation? I think the automatic power down is switched to normal mode by the…
Part Number: MAX3221
Hi team, When auto power-down, how much is the Icc when EN is High or Low? I'd like to know if the Icc changes when the receiver is Enable or disable. Sincerely. Kengo.
Part Number: MAX3221 Hello,
I am looking for some help in determining if there is manufacturing differences between two of the same chips that were ordered at different times. We have an older version that works with our board, but when we purchased a…
Part Number: MAX3221 I was working an issue on one of our PCA's to determine why the RS-232 interface was not working. As I troubleshot, I was thinking it was just a bad chip. So, I replaced the chip. It still did not function correctly. I decided to…
Part Number: MAX3221 I'm working on a circuit that will allow selection between RS-232 and RS-485, by using the EN/FORCEON/FORCEOFF pins of the MAX3221 and SHDN of the MAX13487.
In my tests, while the EN is high, FORCEON is low and FORCEOFF is low…
Part Number: MAX3221 Hi Team,
Do we have time data for this?
FORCEON high, and FORCEOFF also high, given a 3.3 V VCC, how long after FORCEOFF is transitioned to low, is DOUT driving a valid RS-232 level that corresponds to DIN.
Thank you.
-Mark
The MAX3221 stays up because the PC generates a valid RS-232 level.
The MAX3227/TRS3227 automatically powers down when the RS-232 bus has a valid voltage but stays idle for 30 s.
Part Number: MAX3221 Hello,
I don't find the difference between the code MAX3221IDBE4 and MAX3221IDB
What does it mean the E4 in the end of the code ? I don't find this information.
Thanks.
Part Number: MAX3221 Hi team,
As I know, they are the same. TRS is the TI brand name and MAX is the generic brand name.
But the pricing is different on TI website. Max pricing better than TRS.
SoCould I suggest customers use MAX?
Part Number: MAX3221 I use four independent RS232 Tranceiver on a new pcb design and have a lot of errors during transmit. The signal on the RS232 side looks really bad. I increased the value from C8 and C10 to 300nF but it's still not working.I have…