Part Number: MAX3223-EP Team,
My customer had the following request:
I was asked to find out if a socket exists for TI part MAX3223MDBREP that can be installed onto a CCA and used for pre-screening purposes. Do you know if such a socket exists?
…
Part Number: MAX3223E Hi, I'm using MAX3223E as transceiver to debug Uart port and serial application used is TeraTerm or Putty. Issue seen is, after 15-20 minute serial application(Teraterm) is getting hang, it needs restart to get the prints again &…
Part Number: MAX3223 Hi,
Is the temperature change the reason why the maximum current consumption during auto powerdown is 10μA?
Or individual variation?
Best regards,
Part Number: MAX3223 Iam using MAX3223IDBR in my design.
component body marking read to be as
"MB3223I 84KG4 COHP"
What does the 2nd and 3rd line refers to?
Part Number: MAX3223 Hi I am using MAX3223 device in my design. And I have 2 PHYTEC processors in my overall system [ 2 mother boards].
I need to have 2 separate UART/RS232 connectors for getting system logs, one per PHYTEC.
So i need to have UART…
Part Number: MAX3223 Other Parts Discussed in Thread: CD4053B I am using 2 of MAX3223IPW Transceivers in my design and need to mux to another RS232 compatible device.
Do you have any recommendations on any 2:1 RS232 multiplexer?
Part Number: MAX3223E Hi,
When /EN pin is Low, how much is current consumption reduced?
I'm considering to keep /EN High if it is little.
Best Regards,
Kuramochi
Part Number: MAX3223 Other Parts Discussed in Thread: MAX3232E , Hi to all.
I want to simulate MAX3223in HyperLynx 9.4 Software.
To do this, I need IBIS Model it.
Is there it ?
Is it possible to send this model to me?
Thanks.
Part Number: MAX3223E Hi,
I have been asked to find out if this component we purchased has embedded firmware. Additionally, I need to know who manufactured the firmware and where it was manufactured, if it is embedded. The part number I have is MAX3223EIPWR…
Other Parts Discussed in Thread: MAX3223 Hello,
Customer use MAX3223 and test supply current as below while auto power-down enable. But the 2.8mA have load looks large to customer. Do we have any comments or have lower supply current RS232 solution…