Part Number: MAX3223E what are the differences in specification between TRS3223EIDBR (EOL) and MAX3223EIDBR ?
Is there anything needs to be considered, when drop-in replacing TRS3223EIDBR (EOL) with MAX3223EIDBR ?
Part Number: MAX3223 Hi in one application for MAX3223IPW , the force on is connected with invalid bar pin with zero ohm resistor. By mistake the force on is also connected with ground using zero ohm resistor. Initially the ic was working fine, now the…
Part Number: MAX3223E Tool/software: The test found that there is signal input in Pin12/13, but no signal output in Pin17/18. After replacing the chip, the recovery is abnormal. Please kindly check the cause, thank you
Interesting. Thanks for performing that swap.
user4637774 said: According to the RS232 voltage level specification of 5v-15v for identifying 0/1
This is incorrect. The valid range is 3V to 15V. Our transceiver guarantees a minimum 5V output at 3K…
Part Number: MAX3223E Other Parts Discussed in Thread: MAX3223 , Hello team -
TI sent EOL notice for the MAX3223 and recommended the MAX3223E as a pin to pin replacement. Can you tell us what the differences are between MAX3223IPW and MAX3223EIPW. We…
Part Number: MAX3223E Tool/software: Dears:
when customer use below circuit, they found MAX3223E can't use auto power down function, they need pull up forceon pin, then MAX3223E can work. Could you please help check if below circuit is ok ? Thanks.
Part Number: MAX3223E Other Parts Discussed in Thread: TIGER , TVS1401 Hi,
My customer want to have RS232 transceiver with supporting Vrx > 36V, currently MAX13223E could support this requirement.
May I know whether TI have similar part?
According…
Part Number: MAX3223E Other Parts Discussed in Thread: TRSF3221E , TRS3221E , MAX3221E Hi team,
If the use-case is that 2nd channel (DIN2・ DOUT2 ・ RIN2 ・ ROUT2 ) was not used, how can customer to set pins? Open or pull-up to Vcc or pull-down to GND…
Part Number: MAX3223E Hi Team,
Good day. I am posting this inquiry on behalf of the customer.
"I have been experiencing a very high failure rate using this part in a 3.3 volt system. The signature of the failure is an extremely high current draw …
Part Number: MAX3223 I connect 2 MAX3223 transceivers together, I am seeing a sawtooth/rippling waveform on the positive pulse on pin 17 (Tx) output. There is a 6" cable between the RS-232 transceivers. One of the transceivers appear much worst then the…