Part Number: MAX3232E Tool/software: Hi,
We will measure the internal pull down resistor of the RIN1 and RIN2, and we use the avometer connect to the RIN1 and GND,
and our end customer need the measure resistor is more than 5.2Kohm, we know it has the…
Part Number: MAX3232 Tool/software: Hi Team,
We are facing an issue with MAX3232, as the DOUT2 is shorting with GND(becomes 0E wrt GND) when the board is powered ON and a transaction appears on DIN2, we have used NUP2105L for ESD,, and the pin becomes…
JD Heyns said: FIY, we tried a bunch of series resistor values on the actual system and saw that the receivers all work up until +/- 2K2 was added.
Adding larger series resistors on the line will lower the load seen by the drivers. It kind of looks like…
Part Number: MAX3232E Tool/software: If unused channel of TX and RX needed external pull up and pull down for or it has internal pull up and pull down for it. Or it OK to use it as no connect for the unused pin
/resized-image/__size/320x240/__key/communityserver…
Part Number: MAX3232E Tool/software: Hi Texas Instruments (TI) Team,
"MAX3232ECPWR, U1 Low Bias"
At the beginning, we had encountered fail initialize test on related location: U1 (RS232 Driver) at IO board. After we analyze it related to pin3…
Part Number: MAX3232E Other Parts Discussed in Thread: TRS3232E , TRSF3232E Hi Team,
Can MAX3232E guaranteed 230kbps data rate? According to the data sheet, Max data rate is Min 150kbps and Typ 250kbps.
If the answer is no, I’m thinking of proposing TRS3232E…
Part Number: MAX3232 Other Parts Discussed in Thread: TRS3232E , TRS3232 Tool/software: I would like to find the best suitable replacement for obsolete part number DS14C232CM - 2/2 Transceiver Full RS232 16-SOIC. DigiKey suggest MAX3232 series is available…
Part Number: MAX3232 Tool/software: Hello,
I am using MAX3232CDR 16 pin SOIC for RS232 communication. We used 0.1uF MLCC Cap as suggested in datasheet. Supply voltage is 3.3V. It is noticed that IC is working up to 57600 baud rate. When we are checked…
Part Number: MAX3232 Dear Team,
This is Murari Divya from Medha Servo Drives pvt.ltd, we are using the part No : MAX3232MDBREP in our application in between control system to monitor for displaying the control signals.
This part getting problem after…
Part Number: MAX3232 Tool/software: Hello everyone,
I am designing model rocket flight computer for a two stage rocket and I have to use a communication protocol between this two flight computer.
So I desired to use RS232. I have to use MAX3232IPWR for…