Part Number: MAX3232E-Q1 Hello Team ,
Usig MAX3232EIPWR as the interface IC between the UART lines and RS232C components .
Observed the sawtooth pattern waveform on the DOUT lines and RIN lines .
Please suggest proper solution to resolve the issue…
Part Number: MAX3232E-Q1 Hello team,
My customer have below questions regarding C1~C4 in typical application, can you support please?
Vcc=5V, is it okay to use 3V to 5.5V table? They want to use 0.47uF for C2~C4 especially.
Should they consider…
Part Number: MAX3232 Tool/software: HI TI team.
We are experiencing functional issues with the MAX3232CPWR , while the MAX3232CPWRG4 is passing all tests. I would like to confirm if there is any difference between these two components, or if they should…
Part Number: MAX3232 Tool/software: Hi,
I think the following are the causes of IC damage.
・Short circuit of signal line ・Surge ・Noise
In case of MAX3232, if the IC is damaged due to the above reason, could you please tell me how it will behave…
Part Number: MAX3232 Other Parts Discussed in Thread: ESDS452 Tool/software: Hello team,
Based on the below article, SMBJ8.0CA is recommended for MAX3232. I don't understand this because abs rating is lower than Vrms. Can you explain why this part is…
Part Number: MAX3232E Hello Team,
Observed some regular tiny noise in the ROUT 3.3V side of the Max IC. Please clarify what is the route cause of the noise and what is the work around for that. C1+ and C2+ capacitor values are 0.1 micro farad as recommended…
Part Number: MAX3232 Tool/software: In our existing design we have used the part MAX3232IPW line driver . Looking for the drop in replacement for this part . Found the alternate MAX3232IPWR and MAX3232IPWRG . Please confirm the difference between these…
Part Number: MAX3232 Tool/software: For PN# MAX3232MPWREP, we purchased through authorized distributor but trace code showing from TI's certificate does not match with actual marking.
On the actual part marking: 35KAZXO
On the TI certificate: 35AZX0K…