Part Number: MAX3232 We are using TI's RS232C transceiver MAX3232IPWR.
There are serial communication error with s ome of devices.
We find a problem with charge pump circuit inside the device.
Almost devices' charge pump circuits are running about…
Part Number: MAX3232 Other Parts Discussed in Thread: TRS3232E , Hi expert,
Customer has been using MAX3232 IDR but this is an EOLed device. Could you help recommend a P2P device with similar specs? Thanks!
Joyce
Part Number: MAX3232 Dear TI team
I have a question related to the content of the thread below.
https://e2e.ti.com/support/interface-group/interface/f/interface-forum/849803/max3232-floating-pin-questions?tisearch=e2e-sitesearch&keymatch=MAX3232CPW…
Part Number: MAX3232 Whether the 150°C absolute maximum junction temperature mentioned in datasheet is applicable for both commercial and industrial grade parts.
Hi SHH,
I am not sure if you saw the email I sent a couple weeks ago but:
C1 capacitor should be 470nF not 47nF for proper operation of the charge pump.
Tin2 needs to be pulled to VCC or GND as this pin cannot be left floating (the Tout2 could oscillate…
Part Number: MAX3232 Hi,
What is the difference between MAX3232 & MAX3232E? Can I use the IBIS model of MAX3232E for MAX3232? If not, please share IBIS model for MAX3232.
Thanks
Part Number: MAX3232E Other Parts Discussed in Thread: TRS3232E-Q1 Hi team,
My customer designs Outdoor AP application. And their ambient temperature will be up to 95'C at least.
So do we have similar function solution with higher TA specification…
Part Number: MAX3232 Dear Team,
I am facing issue while using the Chipset from the Texas Instrumentation.
Currently, I am using MAX3232IPWR (2/2 Transceiver Full RS232 16-TSSOP) For one of my projects.
While using this IC I have observed that the IC…
Part Number: MAX3232 Hi, had a question about the MAX3232 datasheet. If the VCC is set to 3.3V, what is driver electrical characteristics typically? What is the VOH and VOL voltages when VCC = 3.3V? The reason I ask because under Section 6.6 Electrical…