Part Number: MAX3243 Other Parts Discussed in Thread: GD75232 Hi,
We consider to use MAX3243 to communicate with GD75232 in the diffenert board, and the MAX3243 receive signal from GD75232 is normal but the send a signal to GD75232 is abnormal, the…
Part Number: MAX3243E Hello, we have connected the FORCEON and FORCEOFF pin together through 10k to the same power supply voltage +5V. With that connection everything is working fine.
During start-up of the CPU board the customer saw some signs on the…
Part Number: MAX3243E hi expert
During the operation of MAX3243E, the waveform level of the Driver output signal is abnormal. As shown in the left figure below, it is a normal waveform, and the right figure below is an abnormal waveform. Please help…
Part Number: MAX3243 Hello guys,
One of my customers is evaluatiing MAX3243 using own design PCB board.
When they checked DOUT VOH-IOH characteristics, they found their MAX3243 capavility is lower than Figure 5-1 characteristics. (it is less than…
Part Number: MAX3243E Tool/software: Hi,
I would like to consult about a circuit using the MAX3243ECDBR.
We implemented the attached circuit and observed the following issues:
Even when applying a valid TTL signal to pin 13 (T2IN), no RS-232…
Part Number: MAX3243 Tool/software: Hi,
Currently using MAX3243 16pin TSSOP model.
Whether we can connect Rin - pin4 is directly to 12V Supply.
We are using for COM port connections between PC and Card Reader (CTS - Pin8).
Thanks & Regards,…
Part Number: MAX3243 Other Parts Discussed in Thread: SN75C3243 Hi team,
What's the differences between MAX3243 and SN75C3243? Can they be p2p alternatives?
They have same supply current but SN75C3243 seems support higher data rate, may I know the…
Part Number: MAX3243E Other Parts Discussed in Thread: MAX3243 Tool/software: Hello,
I have never used the MAX3243 before. Could someone review the schematic below and provide any feedback? I know most of the IC pins are omitted and this is intentional…
Part Number: MAX3243 Other Parts Discussed in Thread: TRS3243 , , TRS3243E , Hi team,
Do we have MAX3243CDBR industrial or automotive level version? Thanks!