Part Number: MAX3243 Hello expert,
Based on datasheet page 13, V+ connection could be connected to VCC or GND. My customer would like to know the impact on signal when V+ is connected to GND and VCC. Below post shows the VCC impact but we don't find any…
Part Number: MAX3243E Hello, My customer uses MAX3243E for their new design with Vcc=3.3V. What rated capacitor voltage is required for C1, C2, C3 and C4 respectively at Figure 6 on page 12 in the datasheet? Best regards, K.Hirano
Part Number: MAX3243E Other Parts Discussed in Thread: SN74LVC1G3157 , MAX3232E , TMUX6119 , , TMUX6234 , TMUX6236 , TMUX6219 Hi team, My customer is looking for an RS232 SPDT switch. Could you suggest a device in 2-input/1-output configuration? Sincerely. Kengo…
Part Number: MAX3243 Hi Sir:
Please find the attached is the MAX3243CPWR shcematic PDF file.
Please help review it and kindly revise.
Thank you.
arata_poc_sa_2022091_MAX3243CPWR.pdf
Part Number: MAX3243E Hi,
When FORCEOFF=L, Output is high impedance, but Voltage of Rin pin is reduced. Is this phenomena "normal behavior"? Please advise us.
Also, are there any method to do high-impedance on Rin pin terminal?
Please advise…
Part Number: MAX3243E Other Parts Discussed in Thread: MAX3243 Hello guys,
One of my customers is evaluating MAX3243E which has auto-powerdown mode for their new products.
Their loop-back test (shorted RIN5(No.8 pin) to DOUT3(No.11)) was failed when the…
Part Number: MAX3243 we bought MAX3243CDBR from distributor, the markings are as follows
Line 1: TI 9CAVJKK _G4
Line 2: MAX3243C
Please help us advise the meaning of line 1: 9CAVJKK_G4
Thanks
Addy Low
Part Number: MAX3243E Other Parts Discussed in Thread: MAX3243 , TPS2560 , Hi expert,
My customer is asking that does MAX3243 have UL certificate?
BR,
Oliver
Part Number: TRSF3243 Other Parts Discussed in Thread: MAX3243 , , TRS3243 Hi team,
1. Is TRSF3243 p2p with MAX3243 TSSOP? which one is recommended if they all can support customer's need
2. Do we have complete solution that can support RS-232 RS-485…