Hi Thomas,
Apologies for the delayed response, I was not available last week.
Fragmentation is not currently supported in the software.
Thomas Breitung said: If I comment out the corresponding line in lwip2lwipif.c:241
With this change you are…
Part Number: MCU-PLUS-SDK-AM243X Other Parts Discussed in Thread: SYSCONFIG Tool/software: Hi,
So, I am working on TSN EST and as a starting point I referred to TSN EST example provided in the SDK.
I have connected 2 AM243x LP DUTs directly via Ethernet…
Part Number: MCU-PLUS-SDK-AM243X
Tool/software:
Hello! I am currently working on the Launch Load and Run process for the USB CDC Echo example, but I am running into the following issue:
For some reason, pausing does not work despite being disconnected…
Hi Jayachandran,
Jayachandran Rameshbabu said: In blocking port state, only special packets are permitted to be transmitted and received. For ex: special packets include Peer Delay Messages (used for time synchronization) and Bridge Protocol Data Unit…
Part Number: MCU-PLUS-SDK-AM243X Other Parts Discussed in Thread: SYSCONFIG Tool/software: I'm using AM243X-LP, SDK: 10.01.00.32.
I run the gpio_input_interrupt code, I got the output as mentioned in the document.
Now I'm trying the same procedure…
Part Number: MCU-PLUS-SDK-AM243X Tool/software: Hi,
I've installed a new CCS 20 .
Please tell me how to add my compiler
C:/ti/ ccs1250 /ccs/tools/compiler/gcc-arm-none-eabi-9-2019-q4-major/bin/arm-none-eabi-gcc-9.2.1.exe
I see
but how to change…
Part Number: MCU-PLUS-SDK-AM243X Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
Hi,
I'm using AM243X-LP, SDK: 10.01.00.32.
I run the gpio_input_interrupt code, I got the output as mentioned in the document.
Now I'm trying the same…
Part Number: MCU-PLUS-SDK-AM243X Other Parts Discussed in Thread: SYSCONFIG Tool/software: My application uses two cores (cores R50_0 and R51_0), transferring data between them via IPC and a shared memory region. Both are running FreeRTOS.
The application…
Ivan Ivanenko said: I found the answer about clock configurator, that input clocks are selected for each peripheral. But what if I want to change CPU frequency (for R5F Core)? Is it possible to do it with Sysconfig?
Hello Ivan ,
Typically, all core…
Hi Aaron,
Aaron Thomas said: The values doesn't look right. I don't see the EtherCAT Firmware version in the first 4 bytes and overall it looks different than the expected values. Are you using ICSSG0 or ICSSG1 instance for EtherCAT implementation?…