Part Number: MCU-PLUS-SDK-AM263X Other Parts Discussed in Thread: UNIFLASH Tool/software: Hi TI experts,
I'm trying to run the sbl_qspi_enet application on AM263x. I see that the documentation ( software-dl.ti.com/.../EXAMPLES_DRIVERS_SBL_QSPI_ENET_AM263X…
Part Number: MCU-PLUS-SDK-AM263X Tool/software: Hi Team I am working on adding ethernet libraries and code in empty project. I have added the example of enet_cpsw_tcpclient, while running the example code, it is working fine and link is getting up. I…
Hi vanni vinti ,
If you check the flow, the SBL and HSM Run Time Firmware requires rebuilding when you move from HSFS to HSSE firmware due to change of Root of Trust.
vanni vinti said: For example, do I need to insert the HSM runtime code upload stage…
Deviprasad Nagadavalli said: As per the below link that you have shared with us, why there is a memory overlap between SBL image and application image? [FAQ] AM2634: MCU-PLUS-SDK-AM263X: How to understand/optimize the boot time of RBL/SBL ?
As ROM boots…
Tool/software: HI Ti Team
I am trying to run ADC0 Channel 0 in interrupt mode . While the ADC interrupt is working, the callback function is not being invoked as expected.
Could you please review the code snippet below and let me know what might be…
Part Number: MCU-PLUS-SDK-AM263X https://e2e.ti.com/support/microcontrollers/arm-based-microcontrollers-group/arm-based-microcontrollers/f/arm-based-microcontrollers-forum/1310642/mcu-plus-sdk-am263x-i2c-transaction-failure-after-a-read-to-a-non-existent…
Part Number: MCU-PLUS-SDK-AM263X Tool/software: Hello,
I am using the SDL MCRC module to calculate the CRC value of some input data.
Section 13.6.4.3.4 of the TRM states that it is possible to select the CRC polynomial - but I cannot see how this…
Part Number: MCU-PLUS-SDK-AM263X Other Parts Discussed in Thread: UNIFLASH Tool/software: Hello There,
I want to create a SBL-QSPI for AM263x-cc borad. I have gone through the several examples provide for SBL(seconday boot loader) provide by TI but…
Hi Team,
I am working on AM263x using MCU+ SDK version mcu_plus_sdk_am263x_09_02_00_55 .
I am using UART in callback mode with DMA enabled .
Requirement
My receive length is dynamic:
First, I receive 4 bytes (header).
The 2nd and…
Part Number: MCU-PLUS-SDK-AM263X Other Parts Discussed in Thread: AM2634-Q1 , SYSCONFIG I am working on GPMC using AM2634-Q1 and the device which I am interfacing is a 8bit nor like device which has 16bit addressing. I am not using multiplexed s address…