Part Number: TDA4AL-Q1 Tool/software: Hi, Dear Expert
Because I suffer from display node created failed problem, so I try to use "basic TIDL application" to make sure Display is OK.
HW : J721S2 EVM + DISPLAY 0
SW : SDK 10.0 with default build vision…
Hi Rex,
while waiting your last response I have tried with jffs2. I enabled jffs2 in linux kernel and compiled. I extracted arago-tiny-image-k2g-evm-tax.xz available in sdk and I installed kernel modules into this filesystem and created a jffs2 fs using…
Hi Board designers,
The below links are a quick reference to the collaterals that can be referred when starting a custom design.
Device Selection and features
Product Pages
https://www.ti.com/product/AM3351
https://www.ti.com/product/AM3352…
Hi Karan ,
I load R5F firmwares MCU1_0 and MCU2_0 from OSPI and test it with an application named my_app_linux_arm.But the application run incorrectly and I will post the log below.Can you help me solve it?
Regards!
HJ
1643.boot_log.txt
Part Number: SK-AM62 Hello Ti,
I have built arago project for am62 on ubuntu 18.04 .
with:
https://software-dl.ti.com/processor-sdk-linux/esd/AM62X/08_06_00_42/exports/docs/linux/Overview_Building_the_SDK.html
and the errors are as follow:
ubuntu…
Other Parts Discussed in Thread: TPS65217 Hi,
We are using TPS65217C PMIC with MPU AM335X.
I have below queries regarding PMIC:
1) As per datasheet and user guide of PMIC, output capacitor value used for DCDC1, DCDC2 & DCDC3 is 10UF (shown at…
Part Number: TPS61221 Other Parts Discussed in Thread: TPS61261 Hello urgent help required I have designed a power supply using TPS61221 Booster IC, Input supply is 3V and required output voltage is 3.3V , 7mA. CR2025 coin cell is used to drive circuit…