Other Parts Discussed in Thread: MSP430FR4133 , MSP-EXP430FR4133 , MSP430WARE I just received the MSP-EXP430FR4133 demo board and I have been able to build and run a simple LED blink program, but now I would like to use the LCD. I am using CCS version…
Part Number: MSP430FR2311 Other Parts Discussed in Thread: MSP-EXP430FR2311 Tool/software: Code Composer Studio Could anyone please confirm this. And if it is so- Why?
There are two versions of the project: one in Resource Explorer, and a slightly different…
Other Parts Discussed in Thread: MSP-EXP430FR4133 , MSP430WARE Hi I'm Bharath relatively new to MSP430 and TI's products.
I had bought MSP-EXP430FR4133 to try out some codes and build small products based on it.I did go through the sample codes provided…
Part Number: MSP430FR6047 Other Parts Discussed in Thread: EVM430-FR6047 , MSP-EXP430FR4133
Tool/software:
Greetings of the day!
I wanted to request to please suggest me some part numbers for Panel Mount LCD Display that is compatible with the following…
Hi Tyler,
I took your code and dropped it into a project - since you only provided a small snippet I had to guess at the rest of it to "fill in the blanks". FR4133_LCD_UART_test.zip
Using this code I correctly see "U" displayed on the screen, after…
Hemal Patel said: Please provide EVK part number based on FR4133 to evaluate with BOOST-IR
You can use MSP-EXP430FR4133
Hemal Patel said: MSP430C112
Not recommend to create new design with such old device, if the FRAM is no must to use, I recommend…
Part Number: MSP-EXP430F5529LP Other Parts Discussed in Thread: MSP-EXP430FR4133 no ports enumerated, win10, ccs 10, both updated, or win7, ccs 10 (separated machine) trying to debug msp-exp430f5529lp or msp-exp430fr4133. No USB FET was found and no comports…
Part Number: MSP430FR2111 Other Parts Discussed in Thread: MSP-EXP430FR4133 , MSP430F6779A Hello,
Do you have Software example related to IrDA ?
Thank you
Serkan YILMAZ
Part Number: MSP430FR4133
I have an interesting problem.
I am using the MSP‑EXP430FR4133 and playing with the 32kHz crystal (connected to P4.1 and P4.2) and the RTC.
I set up the RTC in the following way:
RTCCTL = RTCSS__XT1CLK | RTCSR | RTCPS__1…
Part Number: MSP430FR4133 Other Parts Discussed in Thread: MSP-EXP430FR4133
Hey,
I'm currently working on a university capstone project. One of my additional MCUs is the TI MSP430FR4133. I made a pcb to test out the MCU I'm currently looking to verify…