Most of your questions are addressed in the documentation. I would recommend you check out the MSP430 Hardware Tools User's Guide . There are links to it at the top of the MSP-FET430U28 Tool Folder .
Hello Usman,
The MSP-FET430U28 supports MSP430F11x1, MSP430F11x2, MSP430F12x, MSP430F12x2 and MSP430F21xx MCUs in a 28-pin SOIC package (TI package code: DW). This includes all devices you mention attempting to flash. Please make sure that the devices…
Sample code is available for it here .
But there is no LaunchPad or other simple platform to start with this processor. You can use a target board with the MSP-FET:
Or build something on your own using the MSP-FET as programmer/debugger or a LaunchPad…
PIerluigi Rossetti said: please, i need your help, regard the MSP-FET430U28A, it is an KIT Emulator and programmer . My question is: this kit is right for to develop on platform MSP430F2121PW. MSP-FET430U28A has a MSP-FET430UIF and a MSP-TS430PW28A target…
Dan:
Is there a specific reason for using the F1232? (Prior use?)
When you build your PCB, if you use the F1232, you should look at the TI board that will support it, and try to make some room on the board for a JTAG connection. That way, you can…
Hi,
I think I confused with my lengthy question. Let me simplify it with another question.
Lets say I have the MSP430 gang programmer , this programmer has 8 JTAG ports to program 8 MCUs at the same time . Now the target board that I see in TI website…
Well I'm sorry to say that this did not help that much... I followed the instructions and it still did not work, same problem, although I'm not using CCE v3, I use CCE v4. I have an brand new TI Target board an MSP-FET430u28. I guess I have to try out…
Hi,
Thanks for the reply. I was downlaoded this IAR Embedded Workbench Kickstart software from the website which prompted from installed CD. The software descrption as stated below where the GUI without MSP430F4152 device. Any idea for me to download…
I am not sure what package are these F2122 in, but my recommendation is the following: 1. Use a TI Target board & USB FET to program The MSP430F2122IPW devices: http://focus.ti.com/docs/toolsw/folders/print/msp-fet430u28.html
2. See pg 26 of the FET…