Part Number: MSP-ISO Other Parts Discussed in Thread: MSP-EXP430F5529LP , I am connecting the MSP-EXP430F5529LP (launch pad) to MSP-ISO for communication with the EVM430-F6779 Poly-Phase-E-Meter evaluation module. after following the below steps and connecting…
Part Number: EVM430-F6779 Other Parts Discussed in Thread: MSP-ISO , MSP-FET Hello,
So I have this MSP-ISO board and EVM430F67791 energy measurement board with me. Normally we connect the MSP-FET JTAG pins with the evm board directly but how to program…
Part Number: EVM430-F6736 Other Parts Discussed in Thread: MSP-ISO , MSP-EXP430F5529LP Hello,
So I have this EVM430-F6736 for single phase energy measurement and I wanted to link my board with Energy Measurement Design Centre using the given method…
Hi JD,
Some points to high lisght below....
1. I did not power or connect the AC. I was planning to get MSP-ISO to work properly first before I turn on AC. So, I was powering the EVM using the external 3.3V. I don't think the MSP-ISO would be damanged…
Part Number: MSP-ISO Other Parts Discussed in Thread: MSP-EXP430G2ET , , MSP430G2553 , ENERGIA
Hi.
I am using MSP-ISO isolation board with MSP-EXP430G2ET Launchpad to connect it to EVM430-F67641 through RS-232. Question: can isolation board jumpers…
Part Number: MSP430F67791 Other Parts Discussed in Thread: ENERGYTRACE , MSP-ISO Tool/software: Hi all,
I am making a custom board for power measurements using MSP430F67791. I have not used this micro-controller earlier. I am familiar with C2000 microcontroller…
Part Number: MSP430F6779 Other Parts Discussed in Thread: MSP-FET , MSP-ISO Hi, How to debug the meter functionality using CCS if the meter is connected to the 230V supply. or how to test the code whether it is working fine or not in CCS?
regards &…
Part Number: CC2340R2 Other Parts Discussed in Thread: MSP-ISO Tool/software: I need to isolate CC2340 SWD interface.
There is the MSP-ISO that isolates SBW interface for MSP430 devices
What would be the equivalent for the XDS110ET?
Regards,
Part Number: MSP-CAPT-FR2633
FYI
the"CAPTIVATE-ISO Rev C" PCB from the MSP-CAPT-FR2633 Dev Kit has an Silkscreen error on the Target side.
RST/TST signals markings are flipped.
also found the error in the CAPTIVATE-ISO_REV_B_PCB_layers.PDF from…
Part Number: MSP430F6779 Other Parts Discussed in Thread: MSPDS , MSP-ISO , UNIFLASH , MSP-EXP430F5529LP Hi,
I'm encountering an issue where the HID device is detected by the system, but it fails to connect. The device shows up in the device list, but…