I am working on : MSP430F1122 Controller.
Launch Pad : MSP-TS430PW28 Texas Instrumentation Launch Pad.
I am giving giving falling edges within interval of 6 milli seconds, so if any delay by SCS bit it will be tolerable.
Regarding giving edges, i have verified…
Other Parts Discussed in Thread: MSP-TS430PW28 Hi,
I have installed external crystal XT1 32.768kHz on MSP-TS430PW28. I want to test it to know wheather i have installed it correctly or not. if anybody have test code or procedures let me know.
Thanks
Other Parts Discussed in Thread: MSP-TS430PW28 , MSP430F2101 I just tested the supplied Grace examples. "Blink LED from the CPU" is working as intended, but "Blink LED from Timer_A interrupt and CPU" isn't working at all. My LED always stays dark. But because…
Other Parts Discussed in Thread: MSP-TS430PW28MSP-TS430PW28 is one of the DEV tool Suggested in the web but in the product info abt it deliver that it is for 20 & 28 pin soic and TSSop only. but for MSP430F1111AIRGET(VQFN-24) also they…
Jmax604 said:
I would like to evaluate a 28pin 'value line' part, but the launchpad only suports 20pin DIP packages. Are there any socket devices ( https://estore.ti.com/MSP-TS430PW28-MSP430-28-Pin-Socket-Target-Board-P1863.aspx ) that will support…
Other Parts Discussed in Thread: MSP-TS430PW28 I'm trying to debug an out-of-the- box configuration of an MSP-FET430UIF with an MSP-TS430PW28 (Rev.3.1) eval board from the same kit.
The IAR Workbench message is "Fatal error: Could not find device …
Hi Matt,
I've just tried the F2132 with CCSv5.1.0.09000 and an MSP-FET430UIF interface and haven't seen any issues (SBW Mode).
Can you please provide additional information, just to make sure that I'm using the same setup:
Exact CCS build…
Yes that code is correct, originally when debugging a MSP430 already on our product I didn't have P2SEL set correctly. I switched to the MSP-TS430PW28 for ease and couldn't get that to work either. This was due to the zero ohm resistors not being populated…
I'm using a MSP430F2101 with a MSP-FET430UIF (USB Debug Interface) and a MSP-TS430PW28 board. Grace was also used for the configuration.
I want to use P2.5, P2.6 and P2.7 as GPIO Inputs for three digital switches. But I only get an interrupt for P2.5 …
Other Parts Discussed in Thread: MSP-TS430PW28 I need some direction on how to fix a problem regarding 2112 development. I am using the MSP-FET430UIF/MSP-TS430PW28 programming/debugging hardware with IAR Workbench IDE.
This is my problem:
Using the tools…