Part Number: MSP430FR5869 Other Parts Discussed in Thread: MSP-TS430RGZ48C , Hello,
I put MSP430FR5869 on MSP-TS430RGZ48C. MSP430 has uart communication with PC.
MSP430 receives tera term data. After that, the data is sent back to the tera term in…
Hi Sidya:
The supply voltage must be 2V: according to FR5969 DS , Minimum Supply Voltage is Restrictedby SVS Levels, SVS power-up level (max) is 1.99V. So, 2V should be OK.
have the complet diagram: I think you mean the simple hardware setting of…
Hello Anatya,
My recommendation is to use the MSP-TS430RGZ48C target board and a sample of the MSP430FR58671 MCU.
This way your customer can use the actual target device they intend to use in their product and have access to the I2C BSL.
Part Number: MSP430FR5969 Other Parts Discussed in Thread: MSP-TS430RGZ48C , I am using the MSP-TS430RGZ48C development board without the 32KHz crystal oscillator installed. I am trying to get the RTC_B operating, but the only time I get any interrupt…
You seem to be describing a ZIF (Zero Insertion Force) socket board, which you can use to program bare unsoldered devices. This model is what the FR5959 product page points to:
www.ti.com/.../msp-ts430rgz48c
You have to buy a separate socket for…
Part Number: MSP430FR5969-SP Team,
A few common questions Id like to have forum answers to:
We are interested in testing with the launchpad MSP ( http://www.ti.com/tool/MSP-EXP430FR5969 ). If we write code to program this MSP, will the code translate…
I understand that is the MSP430 device derivative but what is it populated on? The MSP-EXP430FR5969, MSP-TS430RGZ48C, or a custom-build EVM? If the MSP-EXP430FR5969 then have you also tried using the on-board eZ-FET?
Regards,
Ryan
Respected Sir,
I am grateful to you for guiding me.I have only MSP430FR5969 lunchPad board.As given in material Slau 657.pdf to load first time MSP-TS430RGZ48C target board is required which i don't have. So I have followed the steps given in Page No…
Hello Srinivasan,
Are you using the MSP-EXP430FR5969 (eZ-FET) or MSP-FET and MSP-TS430RGZ48C target board or some other EVM? If you do not get the prompt to update the emulator again then the update was successful. You can also try updating CCS or…
Hi Martin, Make sure to connect VCC to JTAG pin 2 for FET power or 4 for external power supply, GND to 9, RST to 1, and TEST to 7. Short AGND & DGND, make sure that the microcontroller is oriented properly (i.e. pin 1 is where you expect it), and keep…