Part Number: MSP432P401R Hi community member,
I received the following questions about debugging MSP432P401R and CCS project from my customers.
<Question> 1. When using MSP-FET + MSP-FET-432ADPTR, I think that "connection" of CCS project properties…
Hi Evan,
Thank you for the information.
I will go through the suggestions you have mentioned.
But I see that the link that you have mentioned is related to MSP-TS432PZ100 Rev1.1 board whereas the board that I use is the MSP-EX432P401R. So will this change…
Other Parts Discussed in Thread: MSP-TS432PZ100 Hello,
I examined the wakeup from LPM3.5 and found the first 0x200 bytes of SRAM bank0 memory was cleared or wrote by someone as bellow.
The variable of data and data0 are incremented at lpm3_5 wakeup…
Other Parts Discussed in Thread: MSP-FET , MSP-TS432PZ100 Hello,
Our customer has asked how to use the UART BSL of MSP432P401R Rev-C. So I’ve been investigating about the BSL procedures and I found out I can’t invoke the BSL entry sequence of MSP-FET.…
Hi Michael,
Using P1.1 for HW entry, might not be a good example with the Launchpad, because that pin is not accessible on the Booster Pack header (in other words it will not be easy to pull that pin high). That example was developed using the msp-ts4…
Part Number: MSP432P401R Tool/software: Code Composer Studio
Hello,
Our customer has complained about two troubles of MSP-FET and MSP432P401R as bellow.
1) Step-debug execution can’t work by interrupted from peripherals.
2) PCM check code…
Other Parts Discussed in Thread: MSP-TS432PZ100 , TMDSEMU200-U , MSP-FET Hi,
We are designing debug port for MSP432 prototype board for the XDS200 emulator(TI 14-pin), and we would like to know if the below connection is proper? Especially the TDIS, RTCK…
Hi Benni,
I have not seen this type of error before. Are you connecting the XDS100v2 to a custom board or TI EVM? Please refer to the MSP432 Hardware Tools User's Guide (SLAU571a), which shows the relationship between the ARM 10/20-pin connectors on…
Other Parts Discussed in Thread: MSP432WARE , MSP-TS432PZ100 , MSP-FET Hell,
BSL Scripter v3.1.0 can write an example program, after Factory Reset to the non-blank device.
I had discussed these operations on e2e.ti.com/.../2021272
But under the same operating…
Other Parts Discussed in Thread: MSP-TS432PZ100 , ENERGYTRACE , MSP-FET Hi all,
XDS110-ET exists as a single product?
I want to use the EnergyTrace+ on MSP-TS432PZ100.
In addition, I found the following description.
I think that XDS110-ET is mounted only…