Part Number: MSP430F247 Other Parts Discussed in Thread: MSP-FET Good afternoon, I'm trying to rewrite an MSP43F247 (with blown fuse)
Yes, it can be rewritten with a Softbaugh MSP430 Flash Bootloader
But I need to reschedule with -MSP-FET -MSP430-BSL…
Part Number: MSP432P401R Hi,
I am looking for an application similar to MSP430 flasher for the MSP432. Is there one available? I would like to load a hex file into a MSP432P401R using a MSP FET with a MSP432 adapter.
Thanks,
Jeffrey
Part Number: MSP430F427 Other Parts Discussed in Thread: MSP-FET Hi,
I'm trying to flash MSP430F427 from commands line via JTAG and at the end I've got Exit 16 and Error: unknown device.
Do I use wrong arguments or it's flasher bug? (by the way…
Part Number: MSP430-FLASHER
I found that the write flash bit is not remove when buffer is not full.
Our MSP430 flash was “something” corrupted if I was using CHECK_CRC followed by a SET_PC. Its calling twice flushbuffer, which will force a set WRT which…
Hello Renan,
The post I linked above provides command line hooks for CCS. If you customer just needs to flash the device they can use Uniflash or MSP430 flasher. Uniflash is the newer tool that is actively supported.
FYI you mentioned that you customer…
Part Number: MSP430FR2355 I am trying to flash my MSP430FR2355 with my blinky.c example code after successful compilation However, when I execute MSP430 Flasher, I am getting the error message:
MSP430Flasher: error while loading shared libraries: libmsp430…
Jace H said: If you have disabled the JTAG, and disabled mass erase on wrong BSL password, then your only method to get back into the device is to attempt BSL passwords until the device is unlocked. (That is unless, you disabled BSL access entirely. )…
Part Number: MSP-FET Other Parts Discussed in Thread: MSP430F2370 , , UNIFLASH Hi Support,
i got problems with reprogramming a single memory segment (information memory of MSP430).
Software: MSP FLasher v1.3.20
Hardware: MSP FET FLash Emulation Tool
First…
Part Number: MSP430-FLASHER Other Parts Discussed in Thread: MSP-FET430UIF , MSP-FET Tool/software: Linux hi~ I want to use Mspfet on the Raspberry 2.
I installed mspdebug and etc libs. but it's not working
so I have two questions.
1. Is it possible…