Other Parts Discussed in Thread: MSP430F2003 Hello,
I'm using the MSP430F2003 with the intern 16bit ADC. I want to use serval differential inputs, but how must I configure them?
I want to use channel A4+/-:
SD16INCTL0 = SD16INCH_4; // Enable…
Hello,
This is my first time using thie above part, the JTAG pins aare shared with the SPI pins. Is it possible to use a debugger and the SPI interface at the same time ? or must I program my part then disconnect the JTAG in order to use the SPI interface…
Part Number: MSP430F2003 Other Parts Discussed in Thread: LM4140 Tool/software: TI C/C++ Compiler Hi,
I have implemented analog to digital voltage conversion using the internal reference voltage of msp430f2003 AD16.However, when I use the external reference…
Hi Karthikeyan,
karthi S said: MSP430F2619TPN
For this device, we do not specify a gain or offset drift, rather we only specify the total gain/offset error over the operating temperature. The drift is included within that specification.
karthi…
Part Number: MSP430I2020 Other Parts Discussed in Thread: MSP430F2003 ,
Hello.
I have three questions
1.Could you tell me following values when configuration is the fastest conversion speed in SD24 and SD16 ?
・conversion speed
・resolution that…
The MSP432P401R has a 14 bit ADC. But this resolution is quite uncommon. The MSPs normally have 10, 12, 16 or 24 bits of resolution. The MSP430F2003 has a 16 bit S/D ADC and costs 0.99 $ @ 1000 pcs.
MSP430F2003 and 2013 comes in 4mm by 4mm QFN and have 16bit SAR
TI does have WCSP (Chip scale) 2x2mm, but soldering something that small is only for factories. And probably needs a pre-order of 1K
Running everything on 1.2V Ultra low power: MSP430L092…
Other Parts Discussed in Thread: LMP91000 , MSP430F2003 Hello,
Could someone please tell me what is required to modify the sample MSP430 code for the LMP91000, to work on a Launchpad device:
www.ti.com/product/lmp91000
(Software section)