Other Parts Discussed in Thread: MSP430F2112 , MSP430G2211 , MSP430G2231 I need two PWM outputs the are hardware operated so that there is no CPU overhead.
Device: MSP430F2112
Example code shown for P1.2. Not sure why P1.3 required?
The first…
Other Parts Discussed in Thread: MSP430F2112 , CC2530 I'm using an MSP430f2112 processor and I have some variables that I'd like to have stored in memory after power is cut from the mcu. Can someone please help me with this? I'd also like to do the same…
Other Parts Discussed in Thread: MSP430F2112 Hello Everyone,
I am attempting to create firmware which is capable of over writing the main code (in the flash memory) with new code. After doing some research among these forums, I decided to use the…
Other Parts Discussed in Thread: MSP430F2112 Hello.
I am using MSP430F2112, while code downloading & debugging
2-Wire Spy-Bi-Wire Communication works fine with MSP-FET430UIF (USB) & debugging works well, but when using MSP-FET430PIF (Parallel Port…
Hi All,
Today I test MSP430F2112 for the first time and I can not connect. The IAR log is " No device found, failed to load debugee"
The label is: MSP430F2112 (06K G4 DT2GB ). (TI samples.) The board is our design.
I try the follwings:…
Hi Amalinda, On my shelf one of my MSP circuit powered at end of 2006 is still running from battery(3 AAA pcs), it draw a mere .8uA due it is flashing an led one time a second with very low duty cycle. Battery has lasted his life (best before) on june…
Other Parts Discussed in Thread: MSP430F2112 , MSP430F2274 Hi All,
I am sorry to post another Flash question right after one was previously posted, but the last question didn't help me with my problem that I am running into. I am trying to record…
Other Parts Discussed in Thread: MSP430F2132 , MSP430F2112 , MSP430F2122 Hello,
I am planning to embedded MSP430 Launch pad in my application. I would like to know what is exact fuction for the EEPROM that is used. i.e., U5 'CAT24FC32UI'.
Whether…
Hi John,
the cheapest part I could find WITH the BSL is the MSP430F2112. It is listed in the product selector for $1.10 / pcs. @ 1k pcs.
Rgds aBUGSworstnightmare
P.S. Ti has both; BSL in ROM and in Flash
MSP430F2112:
This message is now displayed when I enter a printf():
Fatal Error[e89]: Too much object code produced (more than 0x1000 bytes) for this package Error while running Linker