Hi Bud,
Sorry, I don't know the details of bootloader code. I'm not sure whether it will erase the code first then to send the ACK.
If it takes about 1s, I think yes.
Eason
Part Number: MSP430F2274 Hello experts,
My customer is looking for MCU similar to MSP430F2274.
Requirement as below;
1. Low power ( less than 1uA at standby mode)
2. Rail to Rail op amp x 2
3. ADC 2ch
Currently, they are considering to…
Part Number: MSP430F2274 Tool/software: Code Composer Studio I want to make a frequency meter but can't enter Timer A.Is there a problem with the software configuration?
#include <msp430.h>
#include "msp430f2274.h"
unsigned int capArray[16] = {0};…
Part Number: MSP430F2274 I have sent a microcontroller MSP430F2274MRHATEP to TI to do failure analysis with Event#QEM-CCR-2307-01286. I have reviewed the report and get confirmation from TI that Pin#15 is short. I have three more question:
1. If there…
Part Number: MSP430F2274-EP Hi,
When debugging my program, I get the same errors on almost each line that says something like "cannot load from non-primitive location." I asked TI about this problem and they told me that the message means that the expression…
Part Number: MSP430F2274 Hello,
I'm having a new 4-wire jtag mode issue. Well its kind of odd and I'm hearing about it from my collegues. I have an fpga that buffers the jtag signal from the pod and it seems that for whatever reason when the pod is…
Part Number: MSP430F2274
Hello,
I am trying to configure pin 7 of the MSP430F2274 micro-controller as the SMCLK output pin, which I can then use to measure the SMCLK frequency.
After referring to the Port P2 Pin Schematic: P2.1, Input/Output With…
Part Number: MSP430F2274 Hello,
Does TI have any information on the expected rise-time/fall-time for MSP430 pins? This information would help me a lot with a noise analysis I am doing.
Thanks!
Part Number: MSP430F2274 Hello Guys,
Good day.
Our customer is planning to use BSL Entry Sequence at Shared JTAG Pins of MSP430F2274. On the datasheet of the device, it was mentioned on Note (1) at page57 that Tools accessing theSpy-Bi-Wire interface…