Configuration 1:
Change to configuration 2
This is the picture of configuration 2:
Can anyone tell me if I can change the configuration 1 to the configuration 2? Configuration 1 is a crystal with 2 terminal. Configuration 2 is a crystal oscillator…
Other Parts Discussed in Thread: MSP430F235 Hello!
I've got a mysterious problem with my ADC12 on my MSP430F235. Independently of using it in single or sequence conversion mode, the ADC seems to be not able to use his full-scale range from 0V to 2.5V …
Other Parts Discussed in Thread: MSP430F135 , MSP430F235 Hi!
I have used the code written for the MSP430F135 on a MSP430F235 and I have found some obstacles. In my code I use these peripherals: flash, gpios on port 1/port2, LFXT1CLK with an external 32,768…
Other Parts Discussed in Thread: MSP430F235 1. While using 64 pin target board MSP-TS430PM64 for msp430f235 some resistor are not connected like R1,R2,R3,R5,R6,R9.............
.So what about these resistor?
Other Parts Discussed in Thread: MSP430F235 , MSP-TS430PM64A 1. I am working with msp430f235 And it is being programmed using msp430FETUIF. May I know that apart from 48 general input and output pins, how rest of the pins should be connected in order to…
Other Parts Discussed in Thread: MSP430F235 1. presently I am working with msp430f235. To get its ACLKi am using external watch crystal .Can this ACLK can be achieved without external crystal oscillator?
2. To install the 32.768khz crystal oscillator…
Other Parts Discussed in Thread: MSP430F235 I am having two questions regarding serial port communication
1. Can we use serial port communication in msp430f235 without using external crystal oscillator?
2. While interfacing msp430f235 with GSM Module…
Other Parts Discussed in Thread: MSP430F235 1. I am having question about the ADC of msp430f235. According to its user guide AVss is kept at zero volt and each pin of microcontroller supports miximum negative voltage -0.3V. if the input analog signal changes…
I am working with msp430 f235. the input signal that is given to ADC12 of msp430 is 150mV sin signal.The negative input voltage range that msp430 can sustain is -0.3V. Would such a input signal can affect the performance of ADC12 ? because the negative…
Other Parts Discussed in Thread: MSP430F235 , MSP430WARE
How to decide speed of clock for ADC12 in case of msp430f235?
Has ADC12 having its different clock for operation?
In TI's code library in all the program related to ADC12 they did not mention…