Part Number: MSP430F2410 I'm using an MSP430F2410 (without DMA) with USCIB0 as an I2C master, and trying to modify the TI_USCI_I2C_master.c code (from app note slaa382a) to support a repeated-start transaction. The code needs to issue an I2C start…
Part Number: MSP430F2410 Tool/software: Code Composer Studio In the file lnk_msp430f2410.cmd, the INT 15 vector is missing, which links to RESERVED 15 @ address 0xFFDE.
Part Number: MSP430F248 Other Parts Discussed in Thread: MSP430F2410
According to:
MSP430F23x MSP430F24x(1) MSP430F2410 www.ti.com SLAS547I – JUNE 2007 – REVISED DECEMBER 2012
Bits 7, 6, and 5 of IFG1 register (0x0002) are "not present".…
Part Number: MSP430F2410
Hi ,
I am trying to perform SW upgrade through BSLDemo ( http://software-dl.ti.com/msp430/msp430_public_sw/mcu/msp430/MSPBSL_Scripter/latest/exports/BSLScripter-3.4.0-windows-installer.zip ) and FTDI cable (C232HD UART cable) ,…
Part Number: MSP430F2410 Other Parts Discussed in Thread: MSP430G2553 Since the P1.1 and P2.2 are used as BSL bootstrap loader to TX and RX.
Could I write a SW UART to use these two ports during application running ? I notice P1.1 and P2.2 are TA0
In the…
Hi ab
I think Reset source is the Multiple source flags on MSP430F248. I think this Reset source and flag are help to you can solve the system issue.
MSP430F23x, MSP430F24x(1), MSP430F2410 Mixed Signal Microcontroller datasheet (Rev. I)
as the comparison…
Part Number: MSP430F2410 Hello,
Posting on behalf of my customer:
I discovered that if I run the ADC12 from the DCO at calibrated 12 MHz, and divide it by 3 (you have register settings to do this) to operate at 4 MHz, the noise and linearity performance…
Part Number: MSP430F2410 Hi,
for our application we use the microcontroller I2C port to communicate with a SFP+, scope is to make some stress tests of this interface,
is it possible modify the I2C timing parameters in order to verify if the SFP+ meets…
Other Parts Discussed in Thread: MSP430F2410 I am using a board created by my hardware engineer, trying to use 4-wire JTAG to program the uC. I am getting the MSP430: Error Connecting to the target: unknown device problem. I will attach the schematic. …