Other Parts Discussed in Thread: MSP430F2419 System Specs: OS: Windows 7 Home Premium 64bit IDE: Code Composer Studio: version 5.1.1.00031 Micro-controller: Using MSP-TS430PM64 target board to program MSP430F2419 Problem Description: I have been using…
Other Parts Discussed in Thread: MSP430F2419 Hi,
I am using MSP430F2419 device which is having ADC12. I using the internal reference voltage(2.5V) and as per the design I have provided two external capacitor 10uF/10V and 0.1uF/10V across VRef+ and VRef…
Other Parts Discussed in Thread: MSP430F2419 I would like to relocate my code currently running in Flash and fLASH2 (MSP430F2419) to extended memory (starting at 0x10000) exclusively. I modified the link cmd file as follows:
.text : {}> FLASH2 /* CODE…
Other Parts Discussed in Thread: MSP430F2419 , TUSB3410 Hi,
Does anyone know if there is a difference between USCI0 and USCI1 on MSP430F2419 UART mode?
My problem is that I have a code for treating received characters via a TUSB3410 converter and…
I am writing a bootloader program that communicates to a PC using the MSP430 UART operating at 9600 baud. Our hardware includes a 32KHz clock crystal which, in the main program, is used to calibrate the DCO at 2.4 MHz via a counter interrupt. The DCO…
Other Parts Discussed in Thread: MSP430F2419 I read through the " MSP430F5438 false breakpoint hits while debugging " and did not notice a response since May. I am also seeing this on the MSP430F2419 which uses the large memory model. What I noticed is…
Hi,
Just a small point I missed in the post above. SPI Slave cannot initiate a transaction. So if MSP430 wants to receive something from an SPI slave it has to perform a "dummy" transmit. That is, you have to write a dummy, say 0x00, in TXBUF. Once…
Other Parts Discussed in Thread: MSP430F2419 I am using MSP430F2419
int main(void) { WDTCTL = WDTPW + WDTHOLD; // Stop watchdog timer while(1) { P1OUT &= ~0x02; }
}
why I cann't put p1.1 to zero?