Part Number: MSP430F2618 Tool/software: We are using the MSP430F2618 chip for a microcontrol system. After power-on initialization, the system reads data from InfoB and InfoD as operational parameters. Once the system stabilizes, these segments are erased…
Part Number: MSP430F2618 Tool/software: Hello,
Problem: Recently, there have been four consecutive cases of high static power consumption after soldering of microcontrollers, with a probability of 1%. The microcontroller model is MSP430F2618TZCAR. …
Part Number: MSP430F2618 Tool/software: Hello,
Does MSP430F2618TZCAR meet functional safety standards? What models of MSP430 series products support functional safety?
Thanks!
Part Number: MSP430F2618
Hello, We are developing a medical device, and as part of this process, we need to catalog all open bugs related to the compiler we are using (TI compiler). As of today, there are some bugs that were reported a few years ago…
Part Number: MSP430F2618 Tool/software: I'm attempting to resurrect an old design with this component on it (obsolete now).
MSP430F2618TGQWTEP
I'm aware it has extended temperature range. This is not needed for the final device. I would like to know…
Part Number: MSP430F2618
Greetings.
I wish to use the low frequency crystal oscillator LFXT1 / ACLK as the source for main processor clock MCLK.
The processor defaults to Digitally controlled Oscillator DCO at start up, and I will code the change…
Part Number: MSP430F2618 Greetings.
We have a data logger based on the MSP430Fx2xx processor using a GSM modem for remote access.
Our GSM code is old 2.5G with GPRS. We are upgrading to 4G. The 4G modem uses the AT command set.
We connect to remote…
Part Number: MSP430F2618
Greetings.
Our MSP430 program includes a bootloader which I have written.
I would like to use the built in BSL, but I haven't access to the BSL pins P1.0 and P1.1 They are used for other things.
Is it possible to access…