Part Number: MSP430F437 Other Parts Discussed in Thread: MSPBSL , , MSP-FET We used JTAG to blow the fuse and cannot program the flash memory by JTAG. However, we need to change the program. Can it be done by BSL TX and RX via off-the-shelf programmer…
Part Number: MSP430F437 Hi team,
Here's some issues from the customer may need your help:
#include <msp430.h>
/** * main.c */ int main(void) { WDTCTL = WDTPW + WDTHOLD; // Stop WDT FLL_CTL0 |= XCAP18PF; // Configure load caps
P2SEL |= 0x30; /…
Part Number: MSP430F437 Other Parts Discussed in Thread: MSP-FET Hello
This is my first experience with micro controllers and I hope I can find an answer on my question.
I have a Pcb board used for water meters based on MSP430F437 mcu. I want…
Part Number: MSP430F437 Hello
This is my first experience with micro controllers and I hope I can find an answer on my question.
I have a Pcb board used for water meters based on MSP430F437 mcu. I want to know if it possible to decode the firmware…
Part Number: MSP430F437 Hello,
I got this question regarding the MSP430F437, 100 pin MCU.
"Is it possible to read all data ROM hex out using SPI pins only ?
Pins:
TDO/TDI 90
TMS 92
TCK 93
And Power 3.3V and GND
do I need to connect also…
Part Number: MSP430F437 Hi
I used to be use MSP430F4371, can I use MSP430F437 to replace without modifying the software and hardware.
I find that they share the same datesheet, and the only difference is F437 has one more ADC12 module than F4371.
Part Number: MSP430F437 do you have thermal characteristics of the msp430f437 in 100 pin lqfp pack. (thermal resistance -junction to ambient and junction to case)
Thanks a lot and best regards
Andrea Brambati
I have used this before. You might try lowering the pull up value. It is easy to breadboard. I don't always trust simulations. You might try putting a resistor I'm parallel with the cap that is 5 to 10 times bigger than your pull up value.
Part Number: MSP430F437
Hi Team MSP430,
My customer requests some additional info/data WRT MSP430F437 errata US13 as follows..
If a receive interrupt occurs during either of the 3 scenarios below, is there is a chance that the micro doesn’t service…
Part Number: MSP430F437 Hi MSP team, My customer is looking for a temperature profile that should be used to attach/solder a device to the board. He recalls seeing this chart in an app note. Would you be able to help me locate this information? Thank…