Part Number: MSP430F4616 On the MSP430F4616 the SVSin pin is shared with P6.7 and Analog Input 7.
I want to use the SVS. Analog 7 is not used. Is setting P6DIR bit 7 to a 0 (input) and P6SEL bit 7 to a 1 all that is needed to enabled the SVSIN?
Thank…
Part Number: MSP430F4616 Tool/software: Hi MSP-Experts,
does the MSP430F4616 support two UART ports? Because the product page is claiming that the device has one UART port only, but when checking the datasheet I see that it has an USCI and an USART…
Part Number: MSP430F4616 Hi ,
My application code size is small(about 6K). I would like to put most code in the lower portion of flash, but would like a couple of ISR's and a BSL program to reside at higher memory location say starting at 0xA000? Is…
Part Number: MSP430F4616 Is there a recommended setting for PxOUT, PxDIR and PxSEL for the pins that are used by the LCD module to achieve the lowest power consumption?
Thank you very much,
James
Other Parts Discussed in Thread: MSP430F449 , MSP430F4616 Hi,
I'v code that run on MSP430F449 .
now I want it to run on MSP430F4616.
I run it under Rowley CrossWorks for MSP430.
under Project properties | Target processor I'v update to…
Other Parts Discussed in Thread: MSP430F4616 Hi
I am using MSP430F4616 processor , I use the built in LCD_A controller of this MCU . We have 32 segments LCD connected to LCD_A controller.
The LCD_A configured with flowing settings
// ****…
Hi, besides the above question, I tried to compile the example code for the custom BSL named 'MSP430F5438A_BSL'. I changed the target in the properties to a MSP430F4619 but I received the following linking errors. They appear to be SFR's I checked the…
Other Parts Discussed in Thread: MSP430F4616 , TRF7970A Hello Sir,
I'm working on the TRF7970A in card emulation mode with Samsung google Nexus 4 mobile. I interfaced the TRF7970A with MSP430f4616 in parallel mode. Initially i faced the problem like…
Other Parts Discussed in Thread: MSP430WARE , MSP430F4616 , MSP430F5438A , MSP430G2001 I'm usinf CCS5.1 to develop code for an MSP430F4616. Since I'm familiar with the StellarisWare package, I was hoping to use the MSP430Ware driver library. However,…
Other Parts Discussed in Thread: CC110L , CC2530 , MSP430F4616 Is any common antenna available for CC110L and CC2530.
I need to make different boards for CC110L and CC2530 with MSP430F4616. And each board should have the same kind of antenna.
Is there…