Other Parts Discussed in Thread: MSP430F47196 Hi,
I have a problem with the SPI communication between CC2480 and the MSP430f47196 device.
When I send a sys_Version request, I get only 0xFF value from the CC2480. I checked different clock settings, MRDY…
Hi everyone,
Can anyone help me !
My question is : Can I use Rogowski Coli sensor instead of CT sensors ?
Is there any code to implement Integrator by software instead of use Hardware Integrator ?
best regards
Hamdy
Other Parts Discussed in Thread: MSP430F47196 Hello,
I am using an MSP430F47196's SD16 to measure mains voltages. The problem I am having is that if the input goes above or below the maximum range of the SD16 (~+-32768), the resulting ADC values do not…
Other Parts Discussed in Thread: MSP430F47197 , MSP430F47196 , MSP430F2013 I use MSP430f47197 and according to its datasheet I have only two hardware UARTs if I am not mistaken! But I need three! Is there any way to get around this problem? Can I write a…
Other Parts Discussed in Thread: MSP430F47196 Hi all,
We had some issues with setting up / configuring interrupts on the MSP430F471 using the latest mspgcc + Eclipse. We were getting a "interrupt vector XX is beyond end of MCU vector table" error when…
Other Parts Discussed in Thread: MSP430F5529 , MSP430F47197 ++++TI members attention please +++++
Just good to know that on the page 72 of the following datasheet "P5.2 (I/O)" on the first line of the bottom table must be "P5.1 (I/O)".…
Other Parts Discussed in Thread: MSP430F47193 , MSP430F47197 , MSP430F47196 I just start to work on an energy meter project. I may use MSP430F47193.
I need some help to choose which IDE I should use, IAR or CCS4.x
I already have CCS4.x Platium. But
…
Other Parts Discussed in Thread: MSP430F47196 Hi
I am using MSP43047196 with a 4-mux LCD..the problem is that in LCD Memory 0 i wrote only 0x01, and it started lighting up all 4 segments connected with S1...same with LCDMEM[0]=0x10, nd with other LCD…