Part Number: MSP430F477 Hello ....
I have post a Question in this forum regarding a delta-sigma converter. I wanted to know whether you can sample DC voltage signals with a sigma-delta converter. My first Post: “For a design with a µC MSP430F477 I need…
Part Number: MSP430F477 Hello ...,
For a design with a µC MSP430F477 I need an AD converter. However, the µC only has a sigma delta converter. Can I convert a DC with the sigma-delta converter?
Best regards Jurgen
Part Number: MSP430F477 Can you clarify what the maximum external Vref voltage is for the device? The spec shows max Vref=AVcc+0.2V in the DAC section and another value listed in the ADC section states max Vref=1.5V.
Regards Bernd
Part Number: MSP430F477 Other Parts Discussed in Thread: TIDM-01000 , TIDA-01504 Hello.
Is it possible to develop HART communication by using integrated DAC of MSP430F477?
Do you have any customers who was able to develop HART Communication by using…
Part Number: MSP430F477 Hi,
The MSP430F477 data sheet does not mention the consumption current when LPM1 is used. I would like to know how much current consumption will be at LPM1.
Best Regards, H.U
Part Number: MSP430F477 Hi community member!
I want to know current consumption of SD16 without internal reference voltage.
I’m looking at MSP430F477 datasheet of SD16_A, power supply and recommended opeating conditions and reference output buffer…
Part Number: MSP430F477 Other Parts Discussed in Thread: MSP430F47177 Dear All ,
I my application i am using I2C Master Transmitter Mode .
I am Facing problem when the following condition :
1 - Acknowledgement BIT is lost or Negative Acknowledgement…
Part Number: MSP430F477 Hi,
Please let me know the following question.
What the value is the input offset voltage of PGA in SD16_A? I believe that PGA in SD16_A should have input offset voltage as well as general Op Amps.
Best regards, Keigo Is…
Other Parts Discussed in Thread: MSP430F477 Hello E2E,
My goal is to jump into the BSL code from an embedded function call. This would allow the firmware image to be updated via the serial port. I have read that certain chips have a customizable BSL…
Dear All,
Could you please help us to understand following errata statement clearly.
Referring to the document "MSP430F47x Device Erratasheet",
Does the statement
"When a flash write or erase is abruptly terminated, any further reliable reads…