Part Number: MSP430F479
Hi,
I am trying to send one byte of data over the UART at a baud rate of 115200 Hz. I am using the BM70 ble module to transfer the data and the baud rate of the BM70 module is also 115200 Hz. I have connected the TX and RX pins…
Part Number: MSP430F479 Other Parts Discussed in Thread: MSP430WARE Dear All,
My Micro controller is getting Rest . And i have troubleshooted the root cause and that is because of the Watchdog timer expiration .
Kindly help me to solve the issue .
…
Part Number: MSP430F479
Hi,
I am facing a little problem with the bluetooth communication with my MSP430F479. I am using the BM70 ble module. I am trying to send two words over the transmit pin and as the buffer can only contain one byte, I am sending…
Part Number: MSP430F479 Team,
we specify the min/typ/max values of SD16GAINx in our datasheet. Theoreticllay 1,2,4,8,16,32. My customer needs the exact value in their application. They measure each units exact gain and offset during production.
Are these…
Part Number: MSP430F479 Tool/software: Code Composer Studio Team,
my customer has developed a custom bootloader and it is at a fixed address. Accordingly, there are interrupt vectors also on a fixed address and pointing to the interrupt addresses.
Pr…
Part Number: MSP430F479 Tool/software: Code Composer Studio Hi,
I need tos et the Reset Vector to my own code, without rts430xxx library functions.
I will write my own bootloader, in a fix memory range in that is also include the interrupt vectors. (0xf000…
Other Parts Discussed in Thread: MSP430F479 Dear Sir
Good afternoon, I used the MSP430F479 DAC, found a phenomenon,
it must be initialized twice, so that the output value is stable All products are available at + - 2 LSB. If the initialization only once…
Other Parts Discussed in Thread: MSP430F479 Greetings,
I'm intersted in knowing if there is a possibility to use some other JTAG programator, precisely OLIMEX ARM-USB-OCD-H for MSP430F479 in IAR? And if not which programator would you prefer. Tnx upfr…
Other Parts Discussed in Thread: MSP430F479 , MSP430F478 , MSP430FG479
I am testing ADC of MSP430F479. I could success in using A3, and A4 analog input
reading from the DAC output.
However, the similar program does not work for A0 and A1 analog input…
Other Parts Discussed in Thread: MSP430F479 Hi,
I have read about the MSP430F47X series Mixed signal micro-controller in this link http://www.ti.com/lit/ds/symlink/msp430f479.pdf.
1) But I am not able find the PIN Name & PIN type information for D5 and…