Part Number: MSP430F5234 The datasheet mentions, "The temperature sensor offset can be significant. TI recommends a single-point calibration to minimize the offset error of the built-in temperature sensor."
What are the steps for a single-point calibration…
Part Number: MSP430F5234 Other Parts Discussed in Thread: MSPBSL Hi,
I try to use the python-msp430-tools (version 0.9.2) to upgrade MSP430F5234's image, but meet some fail.
the tool link as below:
https://pypi.org/project/python-msp430-tools/ …
Part Number: MSP430F5244 Other Parts Discussed in Thread: MSP430F5234 We are selecting A MSP430 as our IOT microcontroller.
And we now have two options, one is MSP430F5244, another is MSP430F5234.
We can see that the main difference of these two…
Part Number: MSP430F5234 On JTAG MSP430 wiki:
MSP430 JTAG interface is not 100% IEEE 1149.1 (JTAG) compatible. For example none of the MSP430 devices has Boundary Scan Cells. We only support the required command BYPASS, but don’t support the other required…
Part Number: MSP430F5234 Other Parts Discussed in Thread: MSP-TS430RGC64C As title. I can't find in MSP430™ Hardware Tools User Guide: slau278ae.pdf, can you please let me know do we have test socket board or not? Thanks.
Regards
Andre
Part Number: MSP430F5234 What does the onboard temperature sensor on the MSP430F5234 measure specifically? i.e. junction temp, ambient temp, die temp, or something else?
Part Number: MSP430F5234 Hi Team
GPN: MSP430F5234
Hi Please can you tell me what is the maximum input leakage or bias current for the Comparator_B input pins of an MSP430f5234. All page & section numbers mentioned below refer to the following datasheet;…
Do you get the same error no matter what code you try to load?
Has this issue been seen on multiple boards as well? If possible, can you swap the IC on a board that has seen the issue and see if the problem persists?
Part Number: MSP430F5234 Other Parts Discussed in Thread: MSP-TS430RGC64C , MSP430F5229 , MSP-FET , MSPBSL Hi,
I want to use I2C for BSL. How can I design the hardware and is there any example code for MSP430F5234 implementing I2C BSL? Thanks.
…
Part Number: MSP430F5234 Other Parts Discussed in Thread: MSP430WARE ,
Tool/software: Code Composer Studio
I installed CCS6.2.0.00050_win32.exe and MSP430Ware_3_60_00_10_setup in windows 7 pc.
I could be able to create and debug projects using the…