Part Number: MSP430F5326
Hi!
The datasheet for part number MSP430F5326IZXHR lists the marking as "F5326", but we found a component marked "MSP430F5326". Is this possible? Best regards, Jack Barret www.chiptronik.hk
Part Number: MSP430F5326 Other Parts Discussed in Thread: MSP430F5526 , Hello
I would like to use a MSP430F5326 as an alternative part for a MSP430F5526, if possible without changing the layout.
We neither use the USB interface of the 5526 nor the…
Part Number: MSP430F5326 We are planning to use MSP430F5326 at 1.8V with PMMCOREVx = 0 and fsystem = 8MHz. What is the minimum voltage level that the 1.8V supply level can go without causing undesired behavior, POR or brownout in the MCU?
Part Number: MSP430F5326
Hello,
I am facing Security violation issue with MSP430F5326.
Is there a way to track this issue?
How could I read what was inside the stack before the security violation?
Can the "Security violation" trigger a UNMI…
Part Number: MSP430F5326 Compiler: IAR 4.21.6
The SPI is set up as slave. Master clock is 312.5 kHz
Observation:
The MISO line is not synchronized to the rising edge of the clock input.
This can rarely happen right after a power-on-reset. It may…
Part Number: MSP430F5324 Other Parts Discussed in Thread: MSP430F5326 , MSP430F5328 Hi Team,
My understand is that the difference between MSP430F5324, MSP430F5326 and MSP430F5328 is only FLASH and SRAM memory size based on the Table 6-1. Device Comparison…
Part Number: MSP430F5326 Hello,
I am trying to compile a code with the renesas ZMOD4410 for a msp430f5326 target. According to Renesas, they used the mspgcc compiler to buid their library so I installed mspgcc GNU V9.3.1.11 and choose this compiler…
Part Number: MSP430F5326 Hello,
I have a question about alternate interrupt vector table in MSP430F532x.
Now my customer is using F5326 and is considering to migrate to F5328 without any S/W and H/W change.
They tested with F5328 and found a big…
Part Number: MSP430F5326 Hello,
What is the quiescent current of the integrated 3.3-V LDO inside the MSP430F5326?
What is the current when no load?
Why is it ON at power on?
Best regards
Mich
Part Number: MSP430F5326 The datasheet for this part does not specify the absolute maximum operating temperature, only the maximum storage temperature (in table 8.1) and the recommended (rather than absolute) operating junction temperature. Could a FAE…