Part Number: MSP430F5336 Other Parts Discussed in Thread: MSP430F437 Hello,
I have two schematics with the only difference that in one I use the MSP430F437 and in the other I use the MSP430F5336.
My problem is, that the schematic with the MSP430F437…
Part Number: MSP430F5336 Other Parts Discussed in Thread: MSP430FR2355 Hi,
Does MSP430F42x0 series support I2C, SPI and UART?
P.S. I am looking for MCU that supports 12-bit DAC, I2C, SPI and UART; With minimum pin count due to space constraint on…
Part Number: MSP430F5336 Other Parts Discussed in Thread: MSP430F155 Hi,
Apart from MSP430F5336, Is there any other small TI MCU with DAC?
Requirement is: Need to convert digital voltage received from slave on I2C to analog voltage (0 to 3V analog…
Part Number: MSP430F5336 We plan to use MSP430F5336 on our design and we have two requirements
1. Have a serial link between MSP430F5336 and the T1042 CPU
2. Be able to upgrade MSP430F5336 firmware over the serial link
To meet the first requirement…
Part Number: MSP430F5336 Other Parts Discussed in Thread: MSP430FR2533 , OMAP-L138 Hi,
We are using msp430f5536 on our custom board and we trying to perform firmware upgrade using BSL (UART).
We can enter BSL by invoking it from software but we are…
Part Number: MSP430F5336
Dear Experts
There is no MSP430F5336 EVM to test DAC.
I saw there is MSP-EXP430FG4618 which can be used but it is pretty expensive and old.
www.ti.com/.../msp-exp430fg4618
Are there any other EVM or Launchpad if customer…
Part Number: MSP430F5336 Hello,
I have a query regarding 16-bit Timer of MSP430F5336 and its associated capture inputs. Is there any possibility of missing the timer overflow interrupt while using the timer module in capture mode?
I am planning to…
Other Parts Discussed in Thread: MSP430F5336 , MSP430F5529 HI
I have setup the UART0 on MSP430f5336 for 1200 baud rate , parity enable,odd parity detection and URXEIE ENABLE. I use assembly language on IAR tool chain for my project .
I need to detect…
Other Parts Discussed in Thread: MSP430F5336 Hi,
When i tried to blow fuse for MSP430F5336, systems shows it is not secured. however, when i tried to connect via JTAG, i always have error #23.
here is the memory option:
what happened? how can…
Other Parts Discussed in Thread: MSP430F5336 , MSP430F168 We have two MSP-FET430UIF one hardware 1.3 and 1.4, both firmware upgraded and both work MSP430F168 devices, only the 1.4 works with the MSP430F5336. We have two MSP-GANG, both work with MSP430F168…