Part Number: MSP430F5340 Hi Team,
Our customer would like to clarify about the positive-going input threshold voltage stated at Section 5.7 of the datasheet of MSP430F534x. Here is his inquiry,
The "Positive-going input threshold voltage" is given as a…
Part Number: MSP430F5340 I understand the voltage abs max for any pin in the device is 4.1V. What happens to the reliability of the micro if a voltage above 4.1V is applied with a resistor in series? If the current is limited to less than 2mA, will the…
Part Number: MSP430F5340 Hi
i am facing an issue where MSP hangs while checking for UCTXSTT bit.
below is my code:
UCB1I2CSA = ucSlaveAddress; UCB1CTL1 &= ~UCSWRST;
UCB1CTL1 |= UCTR | UCTXSTT; // I2C tx, start condition
while (((UCB1CTL1 & UCTXSTT…
Part Number: MSP430F5340
Tool/software: TI C/C++ Compiler
HI
i want to use QAC static code analyser for msp430 compiler
im using ccs => v9.30
msp compiler => ti-cgt-msp430_18.12.4.LTS
may i know the procedure to create a compiler personality?? …
Part Number: MSP430F5340 Hi,
I am working with MSP430F5340 controller interfacing with RRC1120 battery which has a BQ27545G1 .
I am doing the following steps successfully,
1. Sending start condition
2. Sending address.
3. Sending write bit
4. Sending…
Part Number: MSP430F5340 Other Parts Discussed in Thread: MSP430WARE , MSPWARE , BQ27545-G1 Hi
Even i have the same configuration as in linked post -( Dipin's Post )
configuration - MSP430F5340 configured for I2C to communicate with BQ27545 fuel gauge…
Part Number: MSP430F5340 Hi,
We are using Spy-By_Wire mode of JTAG to flash the code in MSP430 in the development stage. But when the device goes into production our mechanical enclosure is ultrasonic welded and we will not have access to the JTAG port…
Part Number: MSP430F5340 Tool/software: Code Composer Studio Dear All,
I would use the vector remapping in RAM for a product develop with
msp430F5342 and compiled with MSPGCC.
Is clear that SYSRIVECT enable remapping RAM at the top and seems correct…
Part Number: MSP430F5340 Other Parts Discussed in Thread: MSP430F5438A Hello,
On page 37 of the datasheet for the MSP430F5340 is shows 470nF hooked to VCORE, but does not give a maximum or minimum.
http://www.ti.com/lit/ds/symlink/msp430f5342.pdf
Would…
Part Number: MSP430F5340 Hello,
My customer is having some issues with MSP430F5340. The issue they are seeing is the program counter goes off to a random address then subsequently triggers a watchdog reset. They are also seeing that Flash can't be programmed…