Part Number: MSP430F5341 Hi,
I have a strange phenomena. In our Boards the bootloader and the firmware erased in several cards.
Just to verify i turn the power on and off for 100 times, and I did not have the phenomena.
Sometimes the bootloader and the…
Part Number: MSP430F5341
Dear Sir,
We have a phenomena that sometimes the boot loader is deleted.
We use the SPY protocol to burn the boot loader.
What might be the reasons for this phenomena?
How can I solve this issue?
Best Regards,
Jiahui
Hi Gray Gao,
So far we have not received any response from the customer. If additional issues arise, I will create a related question.
Thank you for your support.
Best regards, O.H
Part Number: MSP430F5341 Port Mapping and standard IO functions do not allow accessing the RTCCLK for RTC calibration. Can ACLK be used for calibrating RTC?
On the MSP430F5341 it appears the SVS and PMM are hopelessly intertwined. All I want is for the MSP430 (DCO at 12MHz) to be held in reset if the battery VCC drops to 2.1 volts. Does anyone know of a Grace type tool that helps with this setup? I've read…
Other Parts Discussed in Thread: MSP430F5341 Hello,
We have some signal integrity troubles with clock and data signals when programming our MSP430F5341 using Spy Bi-Wire (2 Wire JTAG)
We are using MSP-FET430UIF and connecting as described here http:/…
Other Parts Discussed in Thread: MSP430F5340 , MSP430F5341 , MSP430F5342 hi,
in the following device-specific datasheets, at Table 6-47 the title is wrong:
msp430f5340 www.ti.com/.../msp430f5340 msp430f5341 www.ti.com/.../msp430f5341 msp430f5342 www.ti.com…
Other Parts Discussed in Thread: MSP430F5341 Hi,
It seems the Device Descriptor Table(TLV) is missing from the MSP430F534x datasheet... Can we use the MSP430F535x device's data instead?
Best Regards Prad.
We have some more data about this issue. The conclusion is MSP430F5341/2's behaviour is different from other F5xx devices like MSP430F5310.
In order to cross-check we tried to test the same on TI's target boards with other F5xx devices and the MSP430F5341…
I have a MSP430F5341 with 1.500V (verified) connected to the analog input A3, the internal 2.5V reference selected and am attempting to see A/D conversion results of 2457 counts. (2457 / 4096 * 2.5 = 1.5V)
Here are the two code versions I have tried…