Part Number: MSP430F5438A Tool/software: I'm working with a 5438A running with a 24.576MHz external clock with SMCLK = this rate. when I try to set a baud rate to 921.6Kbps, I get 1,543 Kbps regardless of what I set the UCMTL too. I have verified I can…
Part Number: MSP430F5438A Other Parts Discussed in Thread: TPD2E001 , ESD351 Tool/software: Hi,
We are using MSP430F5438AIPZ controller for our module. one of this UART connecting with external connector to send and receive the data, I would like…
Part Number: MSP430F5438A Tool/software: Hello,
We are currently using the MSP430F5438A XT1 external crystal oscillator 10Mhz.
I looked at the slau208q.pdf manual. When writing about XT1DRIVE, it only talks about the driver configuration in XT1 LF…
Part Number: MSP430F5438A Tool/software: I have created a program that uses 3 SPI and 1 serial interfaces. The program sees the time from debug mode but when I flash it the time is frozen. The time function is part of the TI lib (MSP430F5xx_6xx). It could…
Part Number: MSP430F5438A Tool/software: Hi,
I am facing an issue with the GPIO interrupt function. I am using PORT1 pins 0, 1, and 2, which are pulled up using 1K ohm resistors.
Whenever a pin goes LOW, an interrupt occurs, but now it is triggering…
Part Number: MSP430F5438A Hello,
we have on our board a msp430f5438a, but for a new feature the ram is not suffisant. so I want to know if you have a µC which should have exactly the same pinout but with more RAM.
best regards,
Part Number: MSP430F5438A Hi Team,
I am using MSP430F5438AMPZREP. Please let us know whether its mandatory to use crystals clocks. Can the Microcontroller function without any input clocks.
Part Number: MSP430F5438A
Tool/software:
Hi,
I am currently working with the MSP430F5438A controller. During runtime, a variable is not updating as expected. However, if I place a breakpoint or add a small delay inside the function, the code works…
Part Number: MSP430F5438A
Tool/software:
Hello everyone,
I am developing application for the MSP430, and we need a bootloader. Is it possible to edit the BSL run automatically on every startup without requiring any manual invoke things ? If a specific…