Part Number: MSP430F5519MSP430F5519 code composer studio “Version 12.0.0” shows the error “The debug interface to the target is secure” when debugging with JTAG “MSP-FET430UIF”.
While debugging using code composer studio, the option for security was…
Part Number: MSP430F5519 Could you tell us about the USB function specification for MSP430F5519IPNR?
Although this CPU has USB capabilities 1. Is the signal input (D+, D-) to the USB signal terminal allowed when power is not supplied to the CPU? 2.…
Part Number: MSP430F5519 Hello, I want to store data with micro sd card in my circuit, but I couldn't find a specific sd card connection image for MSP430. I adapted my own micro sd card according to the only image I could find. Can it work smoothly as…
Part Number: MSP430F5519 Hi All
We use MSP430F5519 to build our own products and have applied one VID/PID via filling the form.
http://software-dl-1.ti.com/dsps/forms/vidtracker.html
My question is: may we apply more than one PID?
We would like…
Hi,
I'm assuming you are talking about this thread: e2e.ti.com/.../479569
Unfortunately, we never completed the write-up. Please refer to the points in the noted thread.
Todd
> If your intent is to always be self powered, then i would not plug in a USB cable before the device is setup properly
I should point out, I don't really have control over whether my users plug in one cable first or the other.
Though I can put a…
Other Parts Discussed in Thread: MSP430F5519 Quick question: Does the USB Bootstrap Loader for the MSP430F5519 require an external hardware device/circuit to interface with the USB on a computer? I assume that it is ok to connect the MSP USB peripheral…
I have a customer using a 5519 that is getting an unexpected reset when they turn off an output with a large contactor attached. They have investigated and it is a WDT reset. The contactor is being driven by a small relay on the board that is controlled…
Other Parts Discussed in Thread: MSP430F5529 , MSP430F5519 , MSP430USBDEVPACK Hello,
I have a board with the MSP430F5529 and when I launch the device manager it is recognized as an HID-compliant device with the VID=2047 and HID=0301.
On another…
Part Number: MSP430F5515 Other Parts Discussed in Thread: MSP430F5519 , MSP430F5632 , , TLV320AIC3253 We are looking at these processors - MSP430F5515 , MSP430F5632, MSP430F5519
And these CODECs -
PCM3070IRHBR, TLV320AIC3253IRGER, TLV320AIC33IRGZR…