Part Number: MSP430F6433 Hi Team,
Posting on behalf of our customer.
I'll share this E2E post with our customer so he can reply when needed.
We assemble MSPF430F6433 to our product.
I would like to make sure whether our design is correct or not…
Part Number: MSP430F6433 Other Parts Discussed in Thread: MSP430FR6037 Hello:
MSP430F6433
270 µ A / MHz at 8MHz, 3.0V and flash program execution (typical)
MSP430FR6037
Operating mode: about 120 µ A / MHz
Question: when operating at the same…
Part Number: MSP430F6433 Hi champs,
Could you answer to the below questions about MSP430F6433 SRAM?
Thank you!
Best regards,
Guillaume
Q1: What is the MSP430F6433 technology process (in nm) ?
Q2: What is the MSP430F6433 soft error rate (SER…
Part Number: MSP430F6433 Hi,
one of my customers is looking for the resistor value of the internal resistor ladder of LCD_B. This is required to figure out the current consumption generated by the internal resistors.
Best regards, Phil
Hello uchida-k,
Yes, this is possible. Please refer to the following resources for more detailed information.
SLAA576 Section 4.1.1: www.ti.com/.../slaa576a.pdf
SLAA363 Section 2.2: www.ti.com/.../slaa363a.pdf
SLAA379 Section 8: www.ti.com/..…
Other Parts Discussed in Thread: MSP430F6433 Hello,
My customer is developing health care products using MSP430F6433.
They are creating FMEA of MSP430F6433.
In the process, I have received the inquiry what happens to a damage and functionality when…
Hi JH,
thanks for you support. i resolved this issue now. i made a mistake by the connection of LDOI and VCC. I cut the connection of LDOI and VCC, now the current in LMP3 mode is about 2uA.
Best Regards,
Zhiyu
Think there is an init problem on SPI, I am searching now several hours. Code stays on the first
while(UCB0STAT & UCBUSY){} because UCBUSY is set wit the first Tx-Byte an is not cleard by USCI-B
no signals on SIMO SOMI or CLK ! The ISR is never executed…
Part Number: MSP430F6438 Other Parts Discussed in Thread: MSP430F6436 , MSP430F6435 , MSP430F6433 Hi,
The MSP430F643x series in the 100-pin PZ package comes in four variants
- MSP430F6438 (256kB Flash + DAC)
- MSP430F6436 (128kB Flash + DAC)
…