Part Number: MSP430F6638 I have partioned my main memory into bootloader and Application area. Want try to move interrupt Vector to RAM to execute bootloader with interrupt as smooth and crisp as possible.
I've searched around for real life simpel examples…
Part Number: MSP430F6638 Hey,
Do anybody have complete sample code or link to sample code showing how to enable PU.0 and PU.1 as Output pins and toggle them High-Low.
I am aware of section 42.2.1.3 Port U Control in the MSP430x6xx Family Users Guide…
Part Number: MSP430F6638 I have a 1V dc level applied to an op-amp buffer. The output is then feed through a 1kohm/1kohm voltage divider and then feed to to ADC0 input of the MSP430F3368. Instead of reading 0.5V I get a reading equivalent to 0.7V . When…
Part Number: MSP430F6638
Hi,
I am trying to get my MSP430F6638 to work with Linear Technologies AD7780 which is an ADC. The ADC communicates via a 2 wire SPI connection. I realized when setting up the MSP, it would only allow me to configure the MSP…
Part Number: MSP430F6638 Hi, there
i am trying to use TI-RTOS on MSP430F6638. but i am not able to use TI-RTOS on msp430. for this specific controller is it supported because i am not able to find out any examples. can i get help on this topic.
Part Number: MSP430F6638 Hello Support Team,
Hello Support Team,
I am using MSP430F6638IPZ in my current project. I have a query regarding this. I have a soldered Controller, Decoupling capacitor, 2-wire JTAG, and crystal on my board. I have give external…
Part Number: MSP430F6638 Hi
I've been trying set-up and use I2C and SPI using UCB0 on Port2. The intention is to switch between the two of them during runtime.
The issue I'm facing is that I cannot get the SPI to work after I have enabled I2C(SPI…
Part Number: MSP430F6638 Reposting with less detail but new information.
My device uses the TI USB API in an HID configuration.
When the device is connected to the PC via a USB cable and no apps are open that will communicate with the device, plugging…
Part Number: MSP430F6638 Hello.
When I look in section 9.12.11 of the datasheet there is a table that shows Timer TA0 has a PIN NUMBER for just the ZQW package, but the next section 9.12.12 for TA1 shows the pinouts for both ZCA and ZQW packages. Is this…