Part Number: MSP430F6723 Hi,
I am trying to convert between the RTC registers (in calendar mode) and UTC epoch timestamp, and a bit confused with the results I got so far.
The following my code to set and get RTC calendar time:
// code to set time…
Part Number: MSP430F6723
Hi,
We need to keep one of the input pins high by default, when an external device is connected, that input pin will be driven low by the MCU on external device, as part of the hand-shake process. To reduce power consumption…
Part Number: MSP430F6723 Hi,
in my application I need to generate and read a clock generated by firmware. What is the maximum frequency at which a generic I/O port could opperate. Thank you.
Regards.
Part Number: MSP430F6723 Other Parts Discussed in Thread: MSP-FET , UNIFLASH , MSP430WARE Hi,
I'm new to TI series of microcontroller & JTAG interface. I have designed a board based on MSP430F6723. During software development, my controller got programmed…
Part Number: MSP430F6723 Other Parts Discussed in Thread: MSP-FET Hello,
I am in the middle of development of electricity meter, based on MSP430F6723.
The chip has power supply on DVCC and additional battery on AUX1. The idea is to have the power…
Hey Vsevold,
For DLMS related support, I'd recommend reaching out to Chander G directly via e-mail. I'll also tag him so that he's aware of this thread.
Regards,
JD
I will refer www.ti.com/.../slau319u.pdf for BSL commands
& www.ti.com/.../msp430f6723.pdf in this pdf chapter 6.6 Bootloader (BSL) referring for connections
HI,
Has this issue been resolved? If so, please mark the thread as answered. If there is no response soon, this thread will be closed due to inactivity.
Regards,
Nathan
Part Number: MSP430F6723 Other Parts Discussed in Thread: CC2564MODA Hello team,
Hope you are well and had good time off. Please see below customer question:
MSP430F672xIPN:
What is the typical bluetooth stack size on this processor for the above…