Part Number: MSP430F6723A Other Parts Discussed in Thread: MSP-DSPLIB
Hello.
There is a problem with an SD24 rejection filter in MSP430F6723A.
While measuring voltage 1..5mV on sample frequency 1KHz, we can see a presence of 50Hz signal in SD24 results…
Part Number: MSP430F6723A Dear colleagues,
I need to measure 0...1V signal using SD24B.
Internal reference allows this:
But the question is the stability of this 1V point - if we calibrate our device using only one 1V point, do we comply with Performance…
Part Number: MSP430F6723A 32768 Hz crystal is connected to XT1. For some devices sometimes XT1 becomes to be stopped and REFOCLK starts to be used.
We use following commands to restart XT1:
UCSCTL7 &= ~(XT1LFOFFG | DCOFFG);
SFRIFG1 &= ~OFIFG /* Clear…
Part Number: MSP430F6723A Other Parts Discussed in Thread: MSPBSL Hi,
Beacuse we enabled ecurity fuse procedure of MSP430F6723A . Now need upgrad code for MP MSP430F6723A equipment, how use UART BSL to upgrad?
Thanks!
Part Number: MSP430F6723A Hi, I am looking at the MSP430x5xx and MSP430x6xx family User's Guide. I would like to ask you about the difference between SD24_B and CTSD16.
I think that the major differences between the two ADCs are following points. Is…
Part Number: MSP430F6723A Other Parts Discussed in Thread: DAC7760 , Hi. My customers are considering MSP430F6723A and DAC7760. They want to use MSP430 SPI communication to control DAC7760.
Question: Can we control DAC7760 with the following connections? (DAC7760…
Part Number: MSP430F6723A Hi,
I would like to use a ΔΣ type AD converter(SD24_B) with single-ended input.
The signal level is between 0~3 V. At this time, is it okay to input the same voltage as AVCC to the VREF terminal?
The gain is used…
Part Number: MSP430F6723A Other Parts Discussed in Thread: MSP-FET Tool/software: Code Composer Studio Hi, all,
A software developper said he can not write to MSP430F6723A Flash memory thru JTAG.
In recent days, he tried to write to Flash thru MSP-FET…
Part Number: MSP430F6723A Other Parts Discussed in Thread: MSP430F6723 , MSP430F6736 Hello, can you clarify what the difference between version with and without "A" appendix: MSP430F6723 A IPNR and MSP430F6723IPNR MSP430F6736 A IPNR and MSP430F6736…
Other Parts Discussed in Thread: MSP430F6723A , MSP430F6723 Hi,
Used the RTC of MSP430F6723A , Whether can the independent power supply to RTC module?
P1.0,P1.1 of the MSP430F6723 as the input IO,the MCU power consumption。