Part Number: MSP430F6726A Hi
SMCLK = 8MHz is created by FLL from XT1 = 32KHz and used as the clock of SD24_B.
SMCLK is also used in other modules such as UART.
This time, I want to lower the frequency of SD24_B SMCLK below 8MHz.
However, other…
Part Number: MSP430F6726A Hi,
Please tell me the maximum and minimum values of Vih and Vil
regarding the 32KHz clock from the XIN pin when XT1BYPASS = 1b and XT1BYPASS LV = 0b are set.
The power supply voltage(DVCC) is 3.3V.
Best regards,
Part Number: MSP430F6726A Hi,
My customer s are testing ESD on their board using MSP430F6726A. We have seen the following document.
■MSP430 System ESD Troubleshooting Guide
3.3 Hardware Troubleshooting Guidelines
F igure 2. Recommended SBW Circuit…
Part Number: MSP430F6726A Hi,
My customers want to know the flash life of the MSP430F6726A. Datasheet say "Program and erase endurance 10^4~10^5".
Is there a record of standard deviation?
Regards,
Rei
Part Number: MSP430F6726A Hi,
I have a question about LPM3.5 on MSP430F6726A.
If MSP430 switch to LPM3.5 while using LCD_C,
Are COM and SEG outputs fixed to High/Low at that time?
Regards,
Rei
Part Number: MSP430F6726A Hi,
When a constant voltage is input to SD24_B from a regulated power supply and single conversion is executed,
if the conversion operation is performed multiple times, the result will fluctuate in the lower 4 bits in the…
Part Number: MSP430F6726A
Hi,
My customers use MSP430F6726A. Since the current consumption is high at LPM3, I searched for the cause. When SD24REFS is 1, the current consumption increases. I think this is because it makes 1.2V.
How long is the…
Part Number: MSP430F6726A Other Parts Discussed in Thread: MSP430FE427A Hi,
MSP430 32-KHz Crystal Oscillator Application Note Table 3
I would like to ask you about the safety factor test results.
The safety factors for each crystal of each company…
Part Number: MSP430F6726A Hi
I'm look at "Table 5-36. SD24_B Analog Input"in DS P.64 of MSP430F6726A.
Question 1:
What is minimum value of Input impedance(ZI)? (Because ZID is discription min:300kohm. )
Question 2:
Does the input impedance…