Part Number: MSP430F6736 Tool/software: As the title says, the actual test, found that the voltage, current, power data accuracy is very high, the error is very small; However, the error of the electric energy data is very large, more than 1%. Is the…
Part Number: MSP430F6736 Other Parts Discussed in Thread: MSP430FG479 , MSP-TS430PZ100 , , MSP-FET Hi - trying to find out why I am not able to get MSP-FET430UIF to work with my version of IAR.
I used this interface (IAR/debugging tool) before to debug…
Part Number: MSP430F6736 Can we connect pressure sensor directly to the input of analog pins of MSP430F6736?
We are developing differential pressure transmitter with HART communication. For that we need 24 bit adc for high resolution. Please refer to…
Part Number: MSP430F6736 Hello, customer ask if he needs an external SVS. The User's Guide stated (page 100): "As DVCC ramps up from 0 V at power up, the BOR keeps the device in reset until VCORE is at a sufficient level for operation at the default MCLK…
Part Number: MSP430F6736 Hi team,
customer want to understand that there are some PSSR performance, what's the difference?
Table 5-38 shows SD24_B Performnace and Table 5-47 shows Ref, Build-in Refrence
Part Number: MSP430F6736 单板生产 176PCS EC570 键盘板任务,单板测试发现 13PCS 键盘上电数码管不亮,故障现象如下。
176 pcs of ec570 keyboard boards were produced on the single board. During the single board test, it was found that the nixie tube of 13 pcs of keyboard was not on, and…
Part Number: MSP430F6736 Hi team,
MSP430F6736IPZ chip with single-phase meter in use, 220V, 10 (80) A. The ultimate voltage impact test is currently being performed, applying 120% Un, 70% Un and Un voltages on the voltage line, measuring the maximum…
Part Number: MSP430F6736 Hi experts,
My customer is using MSP430F6736, and they are wondering about Flash on MSP430.
Q1:When accessing Flash memory, is it possible to access (read/write) odd-numbered addresses?
Q2:If so, could you tell me if there…
Part Number: MSP430F6736 Hello,
due to supply chain constrains we would like to switch from MSP430F67 2 6IPN to MSP430F67 3 6IPN.
We have found the table below in the datasheet, showing the differences.
Are there any issues we should be aware of…