Part Number: MSP430F67471A We are trying to understand the differences between the MSP430F67471AIPEU and MSP430F6747AIPEU (The difference between these part numbers being the 1 before the A).
These parts have difference datasheets, so it cumbersome to…
Part Number: MSP430F67471A I have firmware on a MSP430F67471A running at 25 MHz. I would like to write to flash memory during runtime (both information memory and main memory). I have seen that other MSP430 have limits on clock speeds during flash write…
Part Number: MSP430F67471A Other Parts Discussed in Thread: MSP430F67471 , Hi team,
Our customer plans to use MSP430F67471, I received the inquiry about " Unified Clock System" block. According to MSP430F67471's datasheet "5.16 Crystal Oscillator, XT1"…
Part Number: MSP430F67471A I am attempting to load firmware onto the MSP430F67471A using the provided (factory programmed) UART BSL. My understanding is that the RST and TEST pins need to be toggled in the correct sequence to start the BSL. Below is the…
Hi Urica,
I wanted to update you that a solution was reached that involved a kill timer. I enabled the SPI port and DMA, read in 6 bytes to sync it and then, if it failed, the kill timer would reset it. This way, it keeps resetting until the SPI gets…
Part Number: MSP430F67471A Other Parts Discussed in Thread: MSP430F67471 , MSP430F6779 Hello,
We are planning to develop an R&D prototype board with an MSP430F67471 microcontroller. But these component is shown as a non-stocked item in all the vendor…
Part Number: MSP430F67471A Hello.
I have 3 questions about the content of the datasheet In page of 37, 38.
1.Does the indicated graph show the total value of current that can be output at all pins on the microcomputer?
2.Is there data when Vcc is 3…
Part Number: MSP430F67471A Other Parts Discussed in Thread: MSP-FET , MSP-GANG , MSP430-FLASHER
Hello.
I have aquestion.
I am using MSP-FET and MSP Flasher as flash program tool.
Except for MSP-GANG, is the combination of MSP-FET and MSP Flasher the fastest…
Part Number: MSP430F67471A Hello.
I have a question.
When connecting the LCD panel with the same register setting as ILPM 3 LCD, CP described in datasheet page 30, what should be considered in addition to the current consumption shown below?
· ILPM 3…
Part Number: MSP430F67471A
Hello.
I have two questions.
Should I clear REFMSTR bit in REFCTL register when I use LCD Controller with internal reference voltage?
I also want to use ADC10.
I understood REFMSTR must be set at all times when we use…