Part Number: MSP430F6747A Dear Sirs,
Here are the questions about the MSP430F6747A.
1. My customer perform 6KV Air ESD testing and found the MSP430 will reset.
After checked with register data, it was reset by external!
May I know is there any…
Part Number: MSP430F6747A Tool/software: Hello,
We're currently trying to communicate with en eMMC MTFC8GAM thourh the eUSCI SPI interface of the MSP.
Previously we were using an SD card and it worked fine. For testing purpose we used the same PCB…
Part Number: MSP430F6747A Tool/software: Hi,
I've been trying to use DMA for large data transfers at high speed and i came accross an issue when using DMA's interrupts.
My program is trying to send a buffer (9638 bytes) to the eUSCI A0 module configured…
Part Number: MSP430F6747AMSP430F6747A wants to use the internal SD24B function, set the internal reference voltage to 2.5 to -2.5V, how to set; For example, if the value is 2.2V, what should I do
Part Number: MSP430F6747A I am having trouble determining the volts per bit for the SD24_B when it is in offset binary mode.
In Table 29-3 (pg 771) of the MSP430 user guide, the first row shows:
+V_FSR = 0x00FF FFFF
0 V = 0x0080 0000
-V_FSR =…
Part Number: MSP430F6747A Two copies of the program need to be stored and run,However,the program cannot run after modifying MSP430F6747A the flash address
Before modification:
After modification:
Part Number: MSP430F67471A We are trying to understand the differences between the MSP430F67471AIPEU and MSP430F6747AIPEU (The difference between these part numbers being the 1 before the A).
These parts have difference datasheets, so it cumbersome…
Part Number: MSP430F6747A Hello Support member
There is the following description in SLAA666A.(In P3)
3 Addition of RTCLOCK Feature In the MSP430F67xxA devices, a RTCLOCK feature has been added to reduce the amount of reconfigurations that are necessary…
Part Number: MSP430F6747A Using the built-in AD24 bit sampling, the direct voltage acquisition zero drift is about 5,6 mV. The environment is not disturbed, just the bare board test, both of them. Why?
Part Number: MSP430F6747A Hi team,
Fi this issue, please see the figure below:
The left figure is before modification, the right one is after modification.
The customer would like to know how to configure it. Could you help check this case? Thanks…