Part Number: MSP430F6747A Hi, My customer is using MSP430F6747A for production. Customer is planning to update their PCB and some capacitors on board needs to be replaced. Below values are recommended in datasheet. VREF: 100nF(nom) DVCC: 4.7nF(min) AVCC…
Part Number: MSP430F6747A Tool/software: Code Composer Studio Hi, We found the Energy Measurement lib "MSP430-ENERGY-MEASUREMENT". Does customer directly modify iits source code? Also, does TI plan to implement SW for "Neutral missing tampering"? Please…
Part Number: MSP430F6747A
Hi everybody,
I would like to use http://www.ti.com/tool/download/MSP430-ENERGY-MEASUREMENT
now about if this toolkit:
Can perform for higher frequencies, such as 5kHz, which is similar to 50/60Hz?
Does it supports…
Part Number: MSP430F6747A Hi, I have a question from customer about SD_24B operation. Suppose SD_24B is using an external reference voltage (Vref), what happens if Vref voltage level gets decreased? How ADC conversion results are affected by Vref voltage…
Part Number: MSP430F6747A Other Parts Discussed in Thread: TIDM-SINGLEPHASEMETER , MSP430F6736A , TIDA-01094 , TIDA-01088 , TIDM-3PH-ENERGY5-ESD , MSP430F67641A , MSP430F6747 , MSP430F6736 Hello,
We are looking for available firmware resources for Single…
The current that we measured was based on measurements that our entire solution was drawing, including the MSP.
The culprit was the internal ADC Voltage reference, the WD does not reset this / does not switch it off...
Other Parts Discussed in Thread: MSP430F6747A , MSP430F6747 , MSP430F67471 Hi Community member,
Please let me confirm the following question.
[Question.1] Would you please show me the difference between MSP430F6747 and MSP430F6747A?
[Question.2…
Part Number: MSP430F6779A
Hi TI Support,
I suspect about connect capacitor with pin MCU of MSP430F6779A.
Which pin of the mcu if there is no connection to a capacitor? It will cause the mcu to not start-up.
Using 100-Pin PZ Package
Data…
Hello Hattori,
The MSP430F6747 does have some built-in ESD protection but it looks like the max rating is only 1kV, based on the ESD ratings of the datasheet. As the application note and Ti-Designs mention, the MSP430F6747 was improved and can offer…