Part Number: MSP430F67651A Tool/software: Dear All
I am NIBUYA from MACNICA/JP.
Please advise on the following questions:
Customer:Morioka SEIKO
App:Current monitoring devices (sensors)
product:MSP430F67651A
question① Is there an EOL…
Part Number: MSP430F67651A Tool/software: I am trying to run BSL scripts to get the script running, but I am unable to. I am connected to the JTAG connecter on the PCB which has the MSP chip on it. The debug connector(14 pin) connector on pcb is connected…
Part Number: MSP430F67651A Other Parts Discussed in Thread: UNIFLASH , Hi team,
sorry, I am new for MSP430.
OEM Customer got two hex files from their customer. How could OEM customer use them for manufacturing ?
BSLxxx.hex
FWxxx.hex
Could…
Hello,
The BAKCTL is not relevant to MSP430F67651A .
Have you made sure you followed the guidelines in section 5.8.2 Clock Specifications, Table 5-2. Crystal Oscillator, XT1, Low-Frequency Mode. There are a few guidelines at the bottom of the table…
Part Number: MSP430F67651A Hi, I got a question from my customer using MSP430F67651A. He wonders whether it is possible to input high frequency clock (~24MHz) to XT1. Register configuration : UCSCTL1:0021h(DISMOD=1b(Modulation disabled)) UCSCTL4:0000h…
Hi Koichiro,
You can do a quick test on the v5.51.1 compiler. Create a new project with it and see if you can find the MSP430F67651A in the device list.
Best regards,
Cash Hao
Part Number: MSP430F67651A Hi Team, I would like to ask for assistance with our customer inquiry below for MSP430F67651A:
1. What is the value of the internal reference voltage of the 24-bit and 10-bit ADCs of MSP430F67651A when gain = 1?
2. What…
Regarding ...
Carl Hagenmaier said: SDSCM00046695 SDSCM00046115
These appear to be very small floating point computation errors very similar to CODEGEN-4323.
Thanks and regards,
-George
Part Number: ADS1298 Hello,
I have done all the initialization of ads1298 and i can read registers wit POL=1,PHA=0,
when i read channel data which is C00000,8*(800000)
I do not get anything with this setting.
I am receiving wrong register…
Part Number: MSP430F67641A Other Parts Discussed in Thread: MSP430F67651A HI all
i am connect eeprom with
port 1.4 == eeprom SDA PIN
PORT 1.5 == eeprom SCL PIN
because i am use 8 com lcd USB_B I2C as a lcd com pin
please how can ia m configure…