Part Number: MSP430F6779 Other Parts Discussed in Thread: MSP-FET , MSP-ISO Hi, How to debug the meter functionality using CCS if the meter is connected to the 230V supply. or how to test the code whether it is working fine or not in CCS?
regards &…
Part Number: MSP430F6779 Other Parts Discussed in Thread: MSP430F5529 , MSP-EXP430F5529LP Hi,
I am working on my undergraduate final project using the EVM430-F6779 . I installed EMDC and programmed the default firmware for 3 channels at 60 Hz , which…
Part Number: MSP430F6779 Hi, I am working on MSP430F6779 EVM where i want to make the SD24CAL bit in the SD24BCCTLx register where should i make changes to make SD24CAL to 0. regards & thanks
Manish
Part Number: MSP430F6779 Tool/software: Hi Team, 1. With what sampling rate the 24-bit ADCs are working in this MCU?
2. UP tp what harmonic this MCU can calculate accoridngly?
Regards,
Maryam
Part Number: MSP430F6779 Tool/software: HI,
Working on a project which requires to run an application that requires much more than 512KB flash memory that is provided internally MSP430 microcontroller. Is it possible to use an external flash memory…
Part Number: MSP430F6779 Tool/software: Hi Team,
What is the sampling frequency range of the 24-bit Sigma-Delta ADC (SD24_B module) in the MSP430F6779 microcontroller? Up to what harmonic this MCU can calculate with the 24-bit resolution for the ADCs…
Part Number: MSP430F6779 Tool/software: Hi,
Quick question. Is it possible to use F6779 in a power quality application. If i remember correctly there was an example power quality app code available.
Regards
Bilal
Part Number: MSP430F6779 Other Parts Discussed in Thread: UNIFLASH I developed an energy meter based on MSP430F6779. UniFlash refuses to program it with some code of the reference board based on the MSP430F6779I. IAR Workbench can program the code but…
Part Number: MSP430F6779 Other Parts Discussed in Thread: MSPDS , MSP-ISO , UNIFLASH , MSP-EXP430F5529LP Hi,
I'm encountering an issue where the HID device is detected by the system, but it fails to connect. The device shows up in the device list, but…