Other Parts Discussed in Thread: MSP430F6779A I have a project on the MSP430F6779A that uses multimaster I2C. Most of the time it works but occasionally it gets in a state where it can't send data.
What appears to happen is that the UCBBUSY bit gets…
Hello Craig,
Thank you for your detailed post. I'd recommend the MSP430F67xxA family, which includes the F677xA, F676xA, and F674xA devices (you can pick depending on number of peripherals, Flash memory, RAM memory, SD24 channels, etc., required). Take…
Hello Abhi,
I just ran a test using code example msp430f677xA_rtc_01.c, a MSP-TS430PEU128 target board, and a MSP430F6779A device. JP13 was placed in the 3-4 position so that AUXVCC3 was not connected to DVcc and therefore had to be powered by the…
Hey Vikas,
Did you find a way to get this working? I finally tried to quickly recreate the issue on my side but was unsuccessful. This might be a good question for IAR support.
I did find another thread on this topic here: https://e2e.ti.com/support…
Hello,
Sanzheng Yin said: my question is why there is no differential adc driver just like ths4521 to drive the SD24 in MSP430?
The THS4521 appears to be used in audio applications where the required sampling rates can reach up to 192kHz or more.…
Hello Sean,
Thanks for your detailed post. I find it very strange that your ISRs are halting after a certain number of runs. So, the IAR code does not halt after 5,000 runs? It shouldn't. If I remember correctly, the ADC10 gets triggered by the SD24…
The ATMEL part seems to combine a host processor and a communication processor and seems to be an overkill for any smart grid application. However, i would like to understand your entire architecture to ensure we serve your needs to the fullest extent…
Other Parts Discussed in Thread: MSP430F67791A , MSP430F6779A , MSP-FET We have the EVM430-F6779 development board, and I am experimenting with that board but do not succeed everything.
What I have done so far:
I have connected the board with RS232…
Other Parts Discussed in Thread: MSP430F6779A , MSP430WARE Hi everyone,
I have MSP430F6779A (master) which is connected over the I2C to a sleeping (slave) device. The specs of the slave device say, that in order to wake it up, one needs to create SDA…